Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interference between VL53L1X on mobile object.

Interference between VL53L1X on mobile object.We use VL53L1X on mobile objects, and when these objects intersect we have interference between VL53L1X, we have incorrect measurementsIs it possible ? is a misuse of VL53L1XDo you have any examples, solu...

MRIBE.1 by Associate
  • 1374 Views
  • 1 replies
  • 1 kudos

Resolved! VL6180X unstable range results

Hi,Readings from my VL6180X sensor are very unstable. They vary about +-8 mm from measure to measure.I tried with Nucleo board and official api, and also with Arduino board and Sparkfun code. 2,8V power supply is from linear regulator, measured objec...

Cant get VL6180V1 to return ACK on I2C

Hi,i am trying to get STM32F301K8 to communicate with VL6180V1 ToF sensor on my custom board., via I2C (at 20kHz) I had problem getting the API to work so i tried low level I2C access by just sending 0x01 with basic HAL_I2C_Master_Transmit. I noticed...

0693W00000BaWifQAF.png 0693W00000BaWikQAF.png 0693W00000BaWvAQAV.png 0693W00000BaWveQAF.png
KSkor.1 by Associate III
  • 3275 Views
  • 6 replies
  • 0 kudos

VL53L0X crosstalk calibration

Hello. I'm using a VL53L0X sensor with cover glass from www.gilisymo.com, so I need to do crosstalk calibration to get an accurate measurement. The problem is that the correction is too big. The process is as follows: 1) SPAD calibration (ok)2) Ref c...

Resolved! VL53L1X address changing

Hello,We ordered some VL53L1X and put them on our PCB. We ran into a problem at the moment of changing the address: we can give these sensors only two address options 0x52 (default) and 0x53 so that they work correctly, but at other addresses the sen...

AShmy.1 by Associate
  • 5511 Views
  • 1 replies
  • 1 kudos

VL53L1X offset when detaching cover glass

We are using the VL53L1X with the ULD API in our products. During the production process, we perform the offset calibration process as described in UM2510. Our cover glass (Luxycryl red 1600) is actually separated with a light blocker to prevent cros...

mf101 by Associate II
  • 1860 Views
  • 3 replies
  • 0 kudos

Resolved! VL53L1x on breadboard

Hello community,I am trying to implement a simple people counter using a VL53L1X-SATEL on a breadboard with esp32. My problem is that I am confused about the wiring. I've read the data brief but as I am not an expert in electronics I cannot figure it...

KLamp.1 by Associate
  • 1378 Views
  • 2 replies
  • 0 kudos