2022-11-03 5:31 AM
Hi,
I can read the VL53L1X sensor data via i2c. But the values are not consistent when I keep my object from 1cm to 20cm the values are not accurate and not matching with the distance level.
Regards,
Kumar
2022-11-03 6:28 AM
2022-11-03 8:38 AM
Hi Kuma,
Could you please detail your test condition?
Thanks
Julien
2022-11-03 10:45 PM
Hi Julien,
Thanks for your response. Please find my answers as per your queries.
1). Hardware, X-NUCLEO-53L1A1 ? other?
I am using BLE Coretex-M33 Soc module (silab) interfaced via I2C. The data is getting on I2C, But still there is issue with values.
2). SW, ST GUI, other ?
Written the FW logic as per our SoC
3). Is there any additional cover glass?
No additional glass direct values are reading form sensor.
4). Offset calibration has been done ?
Calibration function called every time reading the distance value.
5). Curve measured distance vs actual distance?
Distance measuring in sensor bottom with object
And the detailed resisters and calls c source mentioned in my last thread.
Regards,
Kumar
2022-11-07 3:51 AM
Hi ST Team,
Can i expect the reply as per my below query.
Regards,
Kumar
2022-11-07 7:56 AM
Hi Kumar,
4). Offset calibration has been done ?
Calibration function called every time reading the distance value.
You should not call the calibrations function every time reading distance!
Offset calibration and Xtalk calibration is only called once at start up.
Could you comment the call to see if the ranging data is more consistent.
It is not easy for me to debug your code which is written for another platform than the STM32 Nucleo.
Which version of VL53L1X driver are you using?
I recommend this one called Ultra Lite Driver
Julien
2022-11-09 10:18 PM
Hi Julien
Thanks for you response.
Ok I will do it in one time .
Please let us know the Offset calibration and Xtalk calibration calls in your code?
Regards,
Kumar
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.