Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L1X Reading data

Hi,I can read the VL53L1X sensor data via i2c. But the values are not consistent when I keep my object from 1cm to 20cm the values are not accurate and not matching with the distance level.Regards,Kumar

Akuma.6 by Associate III
  • 1964 Views
  • 6 replies
  • 0 kudos

about schematic for VL53L1X

Dear Sir,We will make our own PCB for VL53L1X application. There are some difference betweenVL53L1X breakout board schematic in UM2359 and VL53L1X schematic in the datasheet.In Figure3 of datasheet, pin 4, 6, and 12 are connected to ground directly....

DSai.1 by Associate III
  • 1276 Views
  • 2 replies
  • 0 kudos

Condensed humidity will affect Time-of-Flight sensors readings?

Hi. I want to measure the water level in an 1.5m height and 1200 litters container. A lot of condensation is created inside it. What if some water droplets are formed in the sensor input and output holes? Would this "water lenses" affect the readings...

XR.1 by Senior
  • 1445 Views
  • 1 replies
  • 0 kudos

Is there any way to know the basic control related commands of the VL53L5CXV0GC chip? Can't the st microelectronics customer technical support center help with this? If neither is possible, should I apply and use only the provided f/w for Eva Board?

I We purchased this sensor to apply it to our own board. I want to know the command to control the sensor on the board, but the data sheet only provides for simple i2c communication and address, index, and data structure.

YJu H.1 by Associate
  • 1419 Views
  • 2 replies
  • 0 kudos

Resolved! Help on issues found in VL53LX API v1.2.8?

I'm using the latest API version (1.2.8) available from the VL53L4CX product page.In my project I have implemented an interface to set configurations or run calibrations.I am also using this driver for both the VL53L4CD and VL53L4CX, since the driver...

AGreen by Associate II
  • 1892 Views
  • 2 replies
  • 1 kudos

Resolved! STSW-IMG035 Minimum Resource Requirements (DMIPS) on HOST MCU

Hi all,i'd like to know the typical resource requirements (mainly required computing power / DMIPS value) of running the TouchLessControl library (STSW-035) library on a host MCU. The GestureEVK-UM.pf mentions a typical RAM and FLASH footprint :I k...

0693W00000Sw5bFQAR.png
LK by Associate II
  • 1966 Views
  • 1 replies
  • 0 kudos

Resolved! Gesture recognition on VL53L5CX?

I have read that ST will be releasing code to show how to do gesture recognition on the VL53L5CX, when is this due to be released?

yzer.1 by Associate II
  • 2887 Views
  • 3 replies
  • 0 kudos

VL53L5CX: minimum size of an empty zone between 2 objects

Hi, I'd like to know what is the minimum size or gap between 2 objects the sensor is able to detect ? My first test shows a surface of 600 cm² seems to be the minimum, i.e a "hole" square of 25 cm x 25 cm or a rectangle of 20 x 30 cm.When I do the ma...

EPARM.1 by Associate
  • 1056 Views
  • 1 replies
  • 0 kudos