cancel
Showing results for 
Search instead for 
Did you mean: 

TOF Sensors VL53 series for LPG level cylinder monitoring

PMato.1
Associate II

Hi all,

We are working on developing an LPG level monitoring system using BlueNRG-LPS MCU and VL53 sensor series.

I am very new to these specific sensors.

Can we have VL53 series installed externally under the metallic cylinder?

Are they also using the principle of acoustic impedence?

Thanks

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
John E KVAM
ST Employee

I know lots about the VL53 sensors and I don't know what acoustic impedance is, so I'm going to guess that is a no. 

And you have to mount these devices behind a Glass, Acrylic, or Polycarbonate window. 

These sensors work by shooting out a flash of light and measuring how long it takes the light to reflect back from a target (Think World War II Radar - but with light.)

It's inexpensive, reasonably low power, and you get an answer in a few millisecond. But you do have to have a way to get the light out - and back in.

- john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
Peter BENSCH
ST Employee

Additionally it must be checked whether the principle of a ToF sensor is suitable because the reflection of LPG may be too small.

You should also carry out extensive tests to see whether you can communicate with Bluetooth out of a metallic container. You may have to switch to LoRa to get at least a few bytes out of the Faraday cage.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
John E KVAM
ST Employee

I'm going to guess that if one were going to do this, it would be to put a window in the tank that the sensor could see through and leave the electronics on the outside. I've tried a lot of liquids, and they all seem to work. But explosive liquid gasses and not something I wanted to try myself. Although I did wonder about it. 

- john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.