Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L5CX TOF

Hi Team, We have our customized projector majorly focused on educational field purpose. Its a short through projector with 16:9 aspect ratio. We are planning to implement Auto keystone and Auto Focus using VL53L5CX TOF sensor. Do you have any driver ...

Deep_bang by Associate II
  • 2149 Views
  • 2 replies
  • 0 kudos

What's VL53L4CX bare driver memory requirement ?

Hi All,I want to port VL53L4CX bare driver to my M0+ MCU (36KB SRAM) however it cannot fit into RAM (.bss)What's RAM requirement of VL53L4CX bare driver ?(I used VL53L1CX ULD and VL53L4CD ULD driver that's ok) or how to trim down the memory requireme...

SLin.11 by Associate III
  • 2594 Views
  • 3 replies
  • 1 kudos

Resolved! VL53L7 Histogram configuration to get all raw histogram bins

 From the user manual "A Guide for Using the Artificial Intelligence Enabler VL53L7CH and VL53L8CH Multizone Time-of-Flight (ToF) Sensors" -- specifically the "Histogram Configuration" section -- it mentions that we can use 'start_bin', 'num_bins', a...

jiantang by Associate
  • 2111 Views
  • 2 replies
  • 1 kudos

VL53L8A at 4m

Hello.Today I will test the VL53L8A evaluation version in the outdoor (cloudy) test data, the code is automatically generated by the STM32Cube. I irradiated VL53L8A to the wall, at about 1.75m, with almost no data. At 4m, the serial port directly sho...

IMG_20240308_102651.jpg
xukong by Associate II
  • 2152 Views
  • 3 replies
  • 0 kudos

Resolved! Can't download STSW-IMG043 for x-Nucleo-53l7a1

Hi,I'm trying to download the STSW-IMG043 software package for VL53L7CH and VL53L8CH.https://www.st.com/en/embedded-software/stsw-img043.html# It fails every time that I try to download. All other packages from the imaging software section are availa...

aroshani by Associate III
  • 8511 Views
  • 12 replies
  • 12 kudos

VL53L3CX and ESP32 weird ranging data

Hi,I am using an esp32 to read out the sensor data of a VL53L3CX. I've tried the example code for the distance sensor and slightly modified it by commenting the if statement out which checks if the distance changed to get continiously data:  #define ...

IMG_1667[13579].jpg Anmerkung 2024-03-25 131929.jpg
PHumm.2 by Associate
  • 2486 Views
  • 2 replies
  • 1 kudos

How to use multiple VL53L5CX Sensors

Hello all,I am having difficulty using multiple VL53L5CX sensors on the same I2C bus on my Jetson Nano. I am able to get a single one working but not multiple. I am following the procedure in the documentation by pulling the LPn low of the sensor I d...

samir6577 by Associate II
  • 3768 Views
  • 4 replies
  • 2 kudos

VL53L4CD not working with black glove

I am trying to use the VL53L4CD sensor in our application, however I am seeing that while using a black latex glove almost on top of the surface (distance of less than 5mm) that it reports distances > 300mm.  It seems to read okay with a range of 10m...

jmueller by Associate II
  • 2715 Views
  • 5 replies
  • 0 kudos

Resolved! VL53L5CX: Entering in LP mode

When powered with 3.6V (both AVDD and IOVDD), VL53L5CX does most of the time does not enter LP mode (via the I2C command).At 3.5V most of the time LP mode is entered correctly, and rarely - incorrectly. At 3.4V, LP mode is entered always correctly.Ac...

Balkana by Associate
  • 2021 Views
  • 2 replies
  • 0 kudos