2023-09-14 4:28 AM
I am using cover glass window IR080C0-IC09-A066-2. I want the design to be IP69. Where I can get the information that the cover glass can withstand If it is subjected to high water pressure (10000 kPa) and high temperature(80*C)?
2023-10-17 4:26 AM
Hello,
The cover glasses are not certified against pressure nor temperature.
Some customers are using them up to 100 degrees and tested it at 1m underwater for 30 minutes but no test were done by ST.
Regards
Anne
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.