cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, what is new about this VD6283 ALS ?

Charlot
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Charlotte MILANETTO
ST Employee

This is the smallest ALS available in the market (Less than 2mm x 1mm), so really easy to integrate.

  • It has 6 channels: Red, Visible, Blue, Green, IR, Clear.
  • It also has Flicker extraction engine. Flicker is a real problem for cameras and for human eyes, so in order to fix that, you can use this information and take really good pictures or films with your camera.
  • Using the Correlated Color Temperature, one can get information about the light and correct for it. Useful for auto adjustment of the screen brightness.
  • And of course it has Lux meter which could be useful to get the illuminance of a scene for example.

It came out on June 2021, all documentations are available on st.com, and product will be orderable starting mid-July 2021.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @Community member​ to the community!

One of the highlights is the light flicker extraction, as mentioned in the datasheet:

With a patented architecture and a high-performance photodiode design, the VD6283

can extract light flickering frequencies to avoid “banding effects�? on videos, or check

that they are safe for human eye. Additionally, the VD6283 is the only sensor able to

extract different light flicker waveforms from 100 Hz and 2 kHz, including LED square

signals, that can run flicker operations simultaneously with ALS operations.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Charlotte MILANETTO
ST Employee

This is the smallest ALS available in the market (Less than 2mm x 1mm), so really easy to integrate.

  • It has 6 channels: Red, Visible, Blue, Green, IR, Clear.
  • It also has Flicker extraction engine. Flicker is a real problem for cameras and for human eyes, so in order to fix that, you can use this information and take really good pictures or films with your camera.
  • Using the Correlated Color Temperature, one can get information about the light and correct for it. Useful for auto adjustment of the screen brightness.
  • And of course it has Lux meter which could be useful to get the illuminance of a scene for example.

It came out on June 2021, all documentations are available on st.com, and product will be orderable starting mid-July 2021.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.