Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to calibrate VL53L0x

Hi,     1》In the dark,Place the white target 140mm from the sensor          call function         Status = VL53L0X_perform_offset_calibration(&vl53l0x_dev,0x8c0000,&pOffsetMicroMeter);     2》In indoor environments ,Place the black target  600mm from ...

zhy by Associate III
  • 937 Views
  • 7 replies
  • 0 kudos

Resolved! VL53L7CX distance data stratification

Hello, I have a VL53 sensor that's outputing distance data but the distance measurements I'm getting are getting "stratified" into about 3 different distances seemingly randomly. I'm using the ULD driver on a custom PCBA with a TM4C1239 microcontroll...

jairo1 by Associate II
  • 440 Views
  • 2 replies
  • 0 kudos

No USB data using X-NUCLEO-53L8-A1 with a Nucleo Board

Hello,  I try to get data from a X-NUCLEO-53L8-A1 board connected to a Nucleo board and visualize it in my computer. If I use the VL53L8CX Gui and connect my COM port and click on the start button, it is working well. However, I would like to get dat...

thogat by Associate
  • 668 Views
  • 3 replies
  • 0 kudos

VL53L0X Arduino vs STM

Hello, I have multiple VL53L0X sensors that I am communicating with over an STM32 board. Two of the sensors started throwing errors (only reading 8191), and so I moved them to an Arduino for the flexibility of using the downloadable API. They worked ...