Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Cleaning TOF sensors

Can TOF sensors such as VL53L1X and VL53L5CX be cleaned with alcohol and/or cleaning wipes or be submerged in cleaning alcohol?

Resolved! Error compiling ToF sensor drivers on Linux - VL53L4CX

I am trying to compile the drivers for the ToF sensor: VL53L4CX for an embedded Linux application. I am running Ubuntu 22.04. When I try to make the drivers I get the following error:   CONFIG_STMVL53LX=m make -C /lib/modules/`uname -r`/build M=$PWD ...

Frooney by Associate
  • 1950 Views
  • 1 replies
  • 0 kudos

Interface VL53L0X with PIC18LF47K42 micro controller

Hi all, I am trying to use a PIC18LF47K42 to read the distance from the Light Ranger 2 click board, which uses the sensor VL53L0X. I copy two folders: core and platform, which are  inside the folder en.STSW-IMG005\VL53L0X_1.0.4\Api I add these file i...

DuyHoang by Associate
  • 2542 Views
  • 3 replies
  • 0 kudos

Resolved! VL6180 Optimal Settings for Acuracy

I am using the VL6180 (not the X version).  This is TOF only.  When reading in continuous mode, I'm getting a tolerance of +/- 1mm and sometimes more.  I'll list my settings below.    My application will measure distances from 10mm to 100mm.  Right n...

gerbers by Associate
  • 1788 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L1X Distance Sensor 50% failure rate (erratic measurements).

Hi,We have an issue with a production build of a VL53L1X based design. The VL53L1X is interfaced to a PIC18F micro, I have inherited the codebase and hardware. The initial production run was for 500 units, of these approx 260 passed our production te...

Aurelius by Associate II
  • 10204 Views
  • 14 replies
  • 1 kudos

Resolved! VL53L8CX no I2C connection

I have a VL53L8CX time of flight sensor connected via I2C on a custom board. The Board has other devices that can talk on I2C no problem. now i cant see the i2c address of the ToF device. from my understanding everything seems to be fine and in accor...

AA.16 by Associate III
  • 2320 Views
  • 1 replies
  • 1 kudos

VL53L5CX initialization fails with ULD driver v1.3.6

I tried using VL53L5CX with ULD API v1.3.6 with an ESP32-S3. I successfully ported the base C function for I2C, as I can talk with the sensor during the first part of the initialization process. Unfortunately, when I reach the NVM part, the function ...

0693W00000YA8JvQAL.png

Resolved! VL53L5CX data is never ready

Hello !I'm working on the VL53L5CX sensor with a Nucleo L432KC.Using the ST example, and after succeeded the initialization of the VL53L5CX, the sensor's data are never ready. In the following function, the p_dev->temp_buffer[1:4] are all equals to 0...

CPoisson by Associate III
  • 3202 Views
  • 4 replies
  • 0 kudos