Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L0X sensor not working

The VL53L0X sensor chips (33 of them) i bought from Digikey isn't working in my PCBA. I tried to use sensor from the module which i purchased early on is working fine in my PCBA & shows distance readings. I suspect the batch had manufacturing defects...

Resolved! RAM based ToF sensors

Hello,I evaluated the VL53L5CX and it works pretty well. Unfortunately I cannot use it in my application because it has a RAM based firmware (flash memory consumption and maybe boot time also).1) Is there a way to easily find out which of the sensors...

PJDE by Associate
  • 1830 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L4CD Cover Panel Design Requirements

Hello all, We will probably need to go for custom cover panels for our sensors, however, we could not find a clear list of requirements to follow.Material: The product's datasheet (DS13812 - Rev 6) states that "the VL53L4CD achieves the best ranging ...

Resolved! Driver version issue for VL53L4CX

HI,The driver file I downloaded from the official website is version 1.2.8.(stsw-img029)But when I downloaded the Demo(X-CUBE-TOF1), I found that it uses version 1.2.10.Should I use the latest one? Thanks

YChen.9 by Associate II
  • 1297 Views
  • 1 replies
  • 0 kudos

Resolved! VL6180 GPIO0 / CE and IIC Address Change

Hello all, We have multiple VL6180 sensors on a common IIC bus.Upon system start up, we are enabling one sensor via its GPIO0 / CE pin, initialising it, changing its IIC address, disabling it, and repeating these steps for all sensors on the IIC bus....

Resolved! VL53L5CX Reponse

I'm having a bit of trouble talking to the VL53L5Cx... I'm appearing to download firmware ok, by all accolunts vl53l5cx_init() is returning with VL53L5CX_STATUS_OK and vl53l5cx_start_ranging() likewise. However, the response on the I2C bus to vl53l5c...

DataNotReady from VL6180

Hi, i am trying to use VL6180 to get an obstacle range.I'm using VL6180 APi to communicate with the device. Communication is ok, and consistent. Each register is written correctly.As show in ST examples I init the device and start a single shot readi...

LDe P.1 by Associate
  • 3446 Views
  • 6 replies
  • 0 kudos

Resolved! vl53l8cx Status always 0 but Distance works and is always different

Hello,i have managed to get the vl53l8cx to run and it returns correct measurements. with the occasional wrong distance. i wanted to take advantage of the "Status" values to throw out bad measurements. however my status prints are always 0.here is my...

AA.16 by Associate III
  • 3365 Views
  • 3 replies
  • 1 kudos

Resolved! TOF Sensor Feasibility

Hello,We are researching the feasibility of a new product and have some questions regarding STMicro's TOF sensors. At this time we are narrowing on the VL53L4CX, but I am sure these questions apply to most of these sensors. The product is detecting d...

jesse-TP by Associate
  • 2220 Views
  • 2 replies
  • 1 kudos