Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L5, data can't ready

Hardware environment: STM32F405 chip and VL53L5CX-SATEL module;Software environment: Based on the STSW-IMG023 sample code, the code is ported to KEIL5 for use;Problem description: After completing the sensor initialization (ranging frequency 10hz, ra...

Philister by Associate II
  • 1030 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L4CD non volatile address change

I am using the VL53L4CD sensor with a nucleo board by using the API provided by ST.By using the xshut pin and the API, I can change the device address.But as soon as I shut down the power or reset the sensor through xshut, its address comes back to t...

lodi12 by Associate
  • 1569 Views
  • 3 replies
  • 1 kudos

VD66GY incorrect coloring

Hi, I am using the VD66GY image sensor on the STEVAL-56G3MAI board. It is connected to an Allwinner S3 with an ISP. This is my v4l2 pipeline:media-ctl --set-v4l2 '"vd56g3 0-0010":0[fmt:SGRBG10_1X10/1120x1360]' media-ctl --set-v4l2 '"sun6i-mipi-csi2":...

sebotics by Associate
  • 876 Views
  • 2 replies
  • 0 kudos

Resolved! Vl53L1X Nonrecoverable Measurement Accuracy Issue

I'm having an issue with a breakout board housing a VL53L1X sensor where, between the breakout board and MCU, the only connections are power, gnd, sda and scl through a PCA9617ADPJ I2C buffer. I've set it up for continuous ranging at about 200ms timi...

otCT by Associate II
  • 2084 Views
  • 4 replies
  • 2 kudos

Resolved! VL53L8CX not working on nrf9151 and getting NAKs

Hi everyone,So I'm trying to get the VL53L8CX ToF lidar working in ZephyrRTOS running on a NRF9151 chip. I'm using the VL53L8CX ULD driver version 2.0.1. The VL53L8CX is connected to the NRF9151 using i2c with the address 0x52, however when I call th...

RobinSuneti_0-1750317865821.png RobinSuneti_1-1750317889367.png RobinSuneti_6-1750319181567.png RobinSuneti_7-1750319207776.png

Resolved! The tof chip anomaly after a long period of non-use

I discovered a strange phenomenon:After I powered on the VL53L4CD, I called the interfaces:The interfaces such as VL53L4CD_SensorInit, VL53L4CD_SetRangeTiming, VL53L4CD_SetDetectionThresholds, and VL53L4CD_SetSignalThreshold complete the initializati...

Blue666 by Associate II
  • 3270 Views
  • 13 replies
  • 0 kudos