2025-08-21 2:21 AM - last edited on 2025-08-21 2:41 AM by Mike_ST
VL53L1CB的最低投资回报率配置是 4x4?我可以将其配置为 1x1 吗?
Translated : The minimum ROI configuration for the VL53L1CB is 4x4? Can I configure it as 1x1?
Solved! Go to Solution.
2025-08-21 10:36 AM
A 4x4 region of interest is about the limit. Each photon strike needs a quench cycle to reset the detector. Any fewer than 16 and it would take forever to get enough photons to get a measurement.
So, alas, 4x4 is the minimum.
It also insures there is enough flexibility for the sensor to adjust the SPADs (detectors.) Not all of them are the same.
- john
2025-08-21 10:36 AM
A 4x4 region of interest is about the limit. Each photon strike needs a quench cycle to reset the detector. Any fewer than 16 and it would take forever to get enough photons to get a measurement.
So, alas, 4x4 is the minimum.
It also insures there is enough flexibility for the sensor to adjust the SPADs (detectors.) Not all of them are the same.
- john
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.