Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L0X I2C Commands

​Can someone point me in the direction where I can find a document giving the I2C register locations to control the VL53L0X. I am trying to read out ranges using an FPGA and the standard I2C bus but all I have found is the device address is 0x52.Than...

RNobe by Associate
  • 4441 Views
  • 3 replies
  • 0 kudos

How to improve color accuracy?

Hi all,I have been experimenting with the X-NUCLEO-53L1A1 and the NUCLEO-F401RE and here are my results. Actual distance White Box Black Box Difference20cm 20.4cm 19.4cm ...

VL6180X measurement in a tube (FoV change?)

We'd like to measure distance in a tube with VL6180X. Tests with a diameter of approx. 5 cm show that the max. distance is reduced and the sensor is underranging. That is probably because the sensor receives some light reflected from the side walls. ...

rastik by Associate III
  • 1782 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L1X reduced FoV

According to the docs I've read maximum FoV using 16x16 SPADs is 27 degrees and minimum FoV using 4x4 SPADs is 15 degrees. But if my math is correct, when side of the measured area is 1/4th then the FoV should be approx. 6.7 degrees. Aren't the SPADs...

rastik by Associate III
  • 2439 Views
  • 2 replies
  • 0 kudos

Resolved! Difference between VL53L1X_Gui and ULD API

When comparing the data sent from VL53L1X ULD and from VL53L1X_Gui I can see some differences.In particular, I was comparing values sent to registers 0x005e and 0x0061 that are used to configure timing budget. I'm not going to write all measurements ...

rastik by Associate III
  • 2499 Views
  • 2 replies
  • 0 kudos

Where to purchase cover glass solutions for the VL53L1X

Hi I was watching this official video on youtube about protective glass covers: https://www.youtube.com/watch?v=BHM2CZVXZGcIn the video there is a mention that the 3D model is available for the protective cover, and I even did see that there is a pro...

RNiel.7 by Associate
  • 3305 Views
  • 3 replies
  • 0 kudos

VL53L1X MBED Library ?

I just got the VL53L1X ToF sensor and I have a k64f board using ARMmbed. I have been searching all day long, but I could not find a library for the board for mbed, does anyone know if there is any library available for this sensor on mbed?

Resolved! I was wondering if it would be possible to add a lens system to the sensor and focus the emitted light and reduce the field of view.

I feel this would solve a couple problems. First, it would allow for more energy to be returned to the detector, increasing the signal to noise ratio and second, it would allow customers to focus on more specific areas. My questions are - can this be...