Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Whether VL53L1X TOF sensor working in sunlight?

I have VL53L1X SATEL development board, I checked the performance of sensor indoors It was accurate and sturdy. But when I checked it outdoors-in sunlight readings varies continuously and haphazardly for steady position of sensor and obstacle. If thi...

YGHAD by Associate
  • 1904 Views
  • 1 replies
  • 0 kudos

Laser power of VL53L0CXV0DH ?

I checked datasheet of part VL53L0CXV0DH, but i cannot find information about laser power. There is description about power consumption of whole device but no data for laser only. We need this information for application certification process.Is ther...

RLee.9 by Associate
  • 989 Views
  • 1 replies
  • 0 kudos

VL53L1X 50 Hz ranging frequency unavailable?

User manual said "It is the fastestminiature ToF sensor on the market with accurateranging up to 4 m and fast ranging frequency up to50 Hz"I could not reach such frequency with all possible tested configuration. The best result was 37 Hz with the val...

Kabron by Associate III
  • 1633 Views
  • 1 replies
  • 0 kudos

GPIO use of VL53L0X

Dear St, I'm using the VL53L0X to detect an object at a distance lower than 30cm. I need that the GPIO is activated (turned down to GND) if an object is present below that distance. If possible it would be better if the sensor is able to detect if th...

CGiov by Associate
  • 2264 Views
  • 1 replies
  • 0 kudos

ROI for the VL53L1X

I'm looking for an example of reducing the ROI with the API for the VL53L1X. I prefer the API released by POLOLU, since I am working with an Arduino, but anything at this point will be greatly welcomed!  POLOLU directed me to your site. From the docu...

GRoes by Associate
  • 1405 Views
  • 1 replies
  • 0 kudos

Device: VL53L1 Subject: VL53L1X_ULD API Question 1: How can I activate the 2V8-interface mode in the compact driver? Question 2: Should register 0x28 and register 0x29 both be written to ensure 2V8-mode?

Explanatory note: The "fat driver" has built in code to detect a "USE_I2C_2V8" flag. If detected, the software writes to register 0x2E. Though the register names for 0x2E and 0x2F suggest that both should be changed to get the interface mode wanted (...

FDuis by Associate
  • 1687 Views
  • 2 replies
  • 0 kudos

VL53L1X I2C no signal

@John E KVAMHi, I want to use the VL53L1X in combination with a Murata CMWX1ZZABZ lora module on the B-L072Z-lrwan1 discoboard.When i try to transmit data using:HAL_I2C_IsDeviceReady(&hi2c1, 0x52, 100, 5);I can see the SCL and SDA signals on my scop...

TVoge by Associate II
  • 2524 Views
  • 1 replies
  • 0 kudos