Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How much surface size is needed for measuring distance by VL53L0X ?

We would like to know sensing distance target's size spec.Our team had tested with some small pole as 1inch diameter and 2 inch height cylinder that put on table.But from upper to bottom as in front of target VL53L0X cannot detect this cylinder dista...

SNish by Associate III
  • 1257 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L0X distance reading varies with reflectivity

I am testing the VL53L0X ability to accurately measuring the distance to objects of different materials and different sizes. The sensor is in continuous mode and I am using VL53L)X_GetRangingMeasurmentData to read the distance and reflectivity value....

BRowl by Associate II
  • 2203 Views
  • 2 replies
  • 0 kudos

Resolved! SPAD zones in VL53L1X sensor

Hello, I have series of questions related to the data implementations using SPAD zone settings. After reading of manuals i made conclusions how to use this feature of the sensor, but i'm not sure if my conclusions are correct.1. I'm interested in acc...

AShmy.1 by Associate
  • 1510 Views
  • 1 replies
  • 0 kudos

VL53L1x: As per the VL53L1x sensor datasheet, slave ID is 0x29. but sensor is responding to 0x4D . Even after XSHUT pin is pulled down , device is responding to slave ID 0x4D.

I have connected VL53L1X sensor to Onion omega2+ controller i2c driver. I2c clock frequency is set to 100khz. For Detecting Slave Devices we have used below command:"i2cdetect -y 0"Output of above command:root@***:~# i2cdetect -y 0   0 1 2 3 4 5 6 7 ...

VNair.1 by Associate
  • 1082 Views
  • 1 replies
  • 0 kudos

VL53L3CX calibration, great difficulty

I've got a custom board with the VL53L3 connected to a Silicon Labs chip. The interface to the sensor works. Saving and restoring calibration data is kicking my ***.My calibration code makes these calls: GPIO_PinOutClear(VL53L3_ENBL_PORT,VL53L3_ENB...

RKreh.1 by Associate
  • 1196 Views
  • 1 replies
  • 0 kudos

Resolved! I2C communication problem with the VL53L1X Time of Flight sensor

Hello,I'm trying to use the VL53L1X on my nRF52DK, but I experience some problems.Previously, I've successfully used the VL53L1X with an Arduino UNO using the pololu Arduino library (link below). For my project I need to use this sensor on the nRF52,...

frank1 by Associate II
  • 3307 Views
  • 2 replies
  • 0 kudos

VL53L3CX Board Compatibility

Hi,Total newb here, so here it goes:I have previously used the Arduino BLE Sense board with a VL53L1X sensor. I am now trying to use 1 (if possible, 2), VL53L3CX sensors from Pololu:https://www.pololu.com/product/3416/blogA couple questions:1.    Can...

DMarq.1 by Associate II
  • 1876 Views
  • 2 replies
  • 0 kudos