Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How have best accuracy at short distances: VL6180 or VL6180X?

Hi!I notice that in the datasheet of both VL6180 and VL6180X, there is EXACTLY the same plot of distance measurement. So that's leaving me to the question: Who is best for short distances, VL6180 or VL6180X?Have a look at page 12/87 here:Proximity an...

DMårt by Lead
  • 3157 Views
  • 2 replies
  • 0 kudos

Resolved! Problem with multiple sensors (3) on the I2C bus and C++ API

Hi ST team and community !I'm here because i have some troubles on the processus of initialisation of multiple sensors VL53L1CB.I use the following library available on gitHub : https://github.com/stm32duino/VL53L1The processus is the following :Shut...

userLM by Associate
  • 1952 Views
  • 2 replies
  • 0 kudos

Resolved! Is it possible to use VL53L0x without X-NUCLEO-53L0A1 extension board, directly connecting to my F302R8 board via I2C? HAL functions(HAL_I2C_Master_Transmit or HAL_I2C_Mem_Write) don't work and all i found is device address 0x52.

My code and console are as presented below. Values are on the console are fixed, they don't change even if i move an object in front of the sensor. Also i dont understand what should i put in "index" byte that is shown in data sheet./* USER CODE BEGI...

0693W00000BZq6tQAD.jpg 0693W00000BZpRMQA1.jpg
BTopb.1 by Associate
  • 2290 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L0X_PerformXTalkCalibration always return zero

Hi All,We foresee cross talk calibration ​for VL53L0X in our application as we are working on enclosure with filter glass on top of VL53L0X .To get understanding of cross talk calibration working, I tried "VL53L0X_PerformXTalkCalibration" with distan...

YGude.1 by Associate II
  • 1743 Views
  • 1 replies
  • 0 kudos

Resolved! Mounting VL6180-SATEL

Given that the VL6180-SATEL breakout board has no mounting holes, is there a preferred method to accurately and rigidly mount it in the desired position and parallel to the mounting surface?I would prefer to have it removable, so a permanent adhesive...

LWill.3 by Associate II
  • 1426 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L1X calibration with cover glass

Hello everyone,I am currently trying to calibrate VL53L1X sensors which are covered by a 4mm thick glass.I am using the ULD from ST to calibrate the offset and xtalk.I achieve a better result with calibration, but I still don't get further than 70-80...

0693W00000APrMKQA1.png 0693W00000APrNwQAL.png
SWand.1 by Associate
  • 2612 Views
  • 3 replies
  • 0 kudos