Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

JYoon.5 by Associate II
  • 2433 Views
  • 4 replies
  • 0 kudos

VL53L5CX API Size "vl53l5cx_buffers.h" seems to be too large for the MCU to handle. Is splitting the buffers ( "VL53L5CX_FIRMWARE[]" )into smaller 'chunks' to send to the SPAD a reasonable solution?

I am trying to use the VL53L5CX with an AVR128DB48. The .h file "vl53l5cx_buffers.h" seems to be too large for the MCU to handle. I think, as it stands, it breaks the 32727 byte limit that AVR is capable of. Is splitting "VL53L5CX_FIRMWARE[]" into sm...

DAzu.1 by Associate II
  • 2332 Views
  • 4 replies
  • 0 kudos

Increasing max FOV angle of latest VL5xxx sensors?

Enjoyed your nice presentation...We need almost hemispherical coverage (maybe 160+ degrees etc) for intrusion/prox detection;we are not power sensitive.Are there optical ways of increasing FOV of the latest 60+ degree FOV sensor to well beyond this F...

BWies.2 by Associate II
  • 1023 Views
  • 2 replies
  • 0 kudos

On the vl5VL53L5cx, the vl3l5cx_check_data_ready function,

 the expected results on the temp_buffer are: if((p_dev->temp_buffer[0] != p_dev->streamcount)            && (p_dev->temp_buffer[0] != (uint8_t)255)            && (p_dev->temp_buffer[1] == (uint8_t)0x5)            && ((p_dev->temp_buffer[2] & (uint8_...

MKhou.1 by Associate
  • 988 Views
  • 1 replies
  • 0 kudos

Resolved! Understanding VL53L5CX Range statuses

If I point my VL53L5CX unit at the ceiling which I have measured to be 2.13m above my device, I get some readings that are status 5 of around 2100 mm and some readings that are status 255 of around 2100mm. Why is this the case? Because 2.1m is within...

VBhat.1 by Associate III
  • 1191 Views
  • 1 replies
  • 0 kudos

the detection rate of SPAD products (VL53L3X)

I'm doing tests on the VL53L3X evaluation board, and trying to reproduce the detection rate issues.In fact, it is hard to get the 50% and 94% valid outcomes out ofcertain large number of tests using the quoted reflection material, ambientlight condit...

旭王.1 by Associate II
  • 2379 Views
  • 4 replies
  • 0 kudos

VL53L0X_PerformOffsetCalibration program example

Hello,Well i have read the documentation on the VL53L0X and it is a clear as MUD with respect to the usage of the function VL53L0X_PerformOffsetCalibration how to use it and why i should use it. I thought these devices where factory calibrated, but i...

Iknig.1 by Associate II
  • 1912 Views
  • 2 replies
  • 0 kudos