Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L3 / VL53L5 calibration for glass with GUI software?

Hello,I want to evaluate VL53L3 / VL53L5 devices. The end application will be behind glass with a distance of ~20-30mm between sensor and glass. I've Nucleo and Satellite boards for the two sensor types and setup a corresponding test environment wher...

RAltm by Senior
  • 2059 Views
  • 3 replies
  • 0 kudos

Measuring short ranges with VL6180

Hi,we are planning to use 3x VL6180 on same PCB to accurately (1mm) measure distances in a dark container. Our required range of measurement is 2 to 80mm. So far we got to around 0.5mm accuracy, but the problem is repeatability. Exactly what i mean i...

KSkor.1 by Associate III
  • 2439 Views
  • 4 replies
  • 0 kudos

I need to detect an object up to a distance of 8 inches 3 times per second with a power budget of 0.1 mW average. I am using a VL53L0X and I have been trying to lower the power consumption without much success. Can somebody help me with this?

I have a design ready to go but it needs to work for 3 years using 4xAA alkaline batteries. My company has planned 500K pcs/yr. I would really appreciate any help with this.Thanks,AL

Tony L. by Associate
  • 1508 Views
  • 3 replies
  • 0 kudos

Resolved! Does the VL53L1X GUI work?

I'm using the X-NUCLEO-53L1A1 and the STM32F401. As the user manual suggests. The GUI opens, but cannot detect the sensor. "Sensor Not Detected. Please ensure sensor connected then Press Black Reset Button on the Nucleo". The X-NUCLEO-53L1A1 is seate...

DAzu.1 by Associate II
  • 1987 Views
  • 2 replies
  • 0 kudos

Resolved! VD6283 GUI Communication Errors

In order to test the X-NUCLEO-6283A1 I installed its GUI (en.VD6283_Setup_v1.0.0.exe).I also installed the ST Link USB driver (as suggested in the GUI Guidelines) and the board is correctly recognized by the host. The GUI seems working fine the very ...

0693W00000FDGuaQAH.png 0693W00000FDH1vQAH.png 0693W00000FDH2pQAH.png 0693W00000FDGzpQAH.png
MFabb.1 by Associate II
  • 3424 Views
  • 6 replies
  • 0 kudos

Very unstable operation of the VL53L0X sensor. It can output 8191/8190 on the first run and output correct values on the second. Please any suggestions how to solve the problem?

Hello. I have problems with VL53L0X sensor. I will list my observations here.First, I carry out the calibration procedure. The sensor passes all initialization steps correctly (Data Init(), Static Init() and so on). Then calibration is performed. For...

histograms with two peaks when detecting a single target

We are using VL53L3CX evaluation board to dig out some information from the histogram.The 24-bin histogram are retreived by calling the Get_AdditionalData function. Two consecutive sets of histograms are got, when we use a white wall as target and th...

0693W00000GY6xLQAT.png
旭王.1 by Associate II
  • 1774 Views
  • 2 replies
  • 1 kudos