cancel
Showing results for 
Search instead for 
Did you mean: 

VD66GY with IMX8M Mini

FB__1
Associate III

Hello ST Brightsense Team,


Would like to know if the VD66GY Linux driver (STSW-IMG503_V4L2) will work on an NXP IMX8M Mini (no hardware ISP) ?  If not will it work with the IMX8M Mini Plus (with Hardware ISP).

Currently using the STEVAL-66GYMAI.
In the STSW-IMG503_V4L2 package, the provided driver / device tree seems for the Raspberry PI, what would be the required changes for that to work on NXP IMX8 platform ? Is the vd56g3.json ISP tuning file required ( no libcamera installed, only using Gstreamer)...

 

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions
CyrilTechPro
ST Employee

Hi FB__1, 

We are pleased to confirm that all the provided image sensor drivers are fully compatible with Linux kernel version 6.1.x.

Regarding the IMX8M platform, support for integration is not yet available at this time. However, we are actively monitoring developments and will keep you promptly informed as soon as support becomes available to assist with your project needs.

 

 

Regards 

View solution in original post

4 REPLIES 4
FB__1
Associate III

Hello,
Is STSW-IMG503_V4L2 driver provided by ST tested and working on Linux kerne 6.1.x with V4L2 ?
Thank you.

CyrilTechPro
ST Employee

Hi FB__1, 

We are pleased to confirm that all the provided image sensor drivers are fully compatible with Linux kernel version 6.1.x.

Regarding the IMX8M platform, support for integration is not yet available at this time. However, we are actively monitoring developments and will keep you promptly informed as soon as support becomes available to assist with your project needs.

 

 

Regards 

FB__1
Associate III

Is the vd56g3.json ISP tuning file required ( no libcamera installed, only using Gstreamer) ?
Where should i put it if it is needed ?

FB__1
Associate III

Hello @CyrilTechPro ,

From https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/206209/1/AN13713(8MP%20ISP%20New%20Camera%20Porting).pdf 

 

"In addition,
get the camera calibration files (.xml), dewarp calibration files (.json), and sensor-
configuration files (.cfg) ready to set correct ISP parameters and stream mode."

 

Where can i find those files for the ST - VD66GY camera ?

 

Thank you.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.