Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.
After been testing VL53L3CX in my own board based in a STM32F407 micro, I want to test VL53L1CB now. But I am not wiring (satellite board) to a Nucleo board. I have connected it to my own board and trying to reformulate the project with STM32CubeMX. ...
Range Status value 3 is "Min Range Fail", which is checked by reading from VL53L0X_REG_RESULT_PEAK_SIGNAL_RATE_REF.What is the Peak Signal Rate Ref.?I'm finding how to differentiate between a reflective sheet and a high gloss stainless steel like a ...
As you know, the reflective sheet is very bright regardless of the reflective sheet surface angle.However other reflective materials, such as mirrors, are only bright when the surface angle is perpendicular to the VL53L0X.In such cases, it is diffic...
Hi. We are starting a new automation project that needs to detect distance to objects as small as 5 cm by 5 cm, at a distance from 5 cm up to 200 cm. I have been testing VL53L3CX, and VL53L1 through Satel eval. boards. Connected to a proprietary hard...
In the example file there is this comment. /* (Optional) Change the min and max distance used to detect motions. The * distance between min and max must never be >1500mm, otherwise the function below returns error 127 min value is 400 max v...
I would to know how can I read 16bits response to this device from linux?
Hello,I have a uni project which involves VL53L0X ToF sensor, at first I thought it is easy I2C sensor, but when learning about it, found out that I was wrong . As I understood this sensor requires API to run it, but i cant find anywhere on the ...
The Datasheet describes that if the sensor is powered and the XSHUT is active, then the sensor is in HW Standby mode. It seems that in my case, the sensor does not always work correctly after exiting XSHUT mode. It can give errors RangeStatus = 2, Ra...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.