2020-04-23 7:07 AM
Good afternoon. I bought myself Teseo LIV3R and LIV3F modules. Download the HAL library and errors are generated when compiling the kernel:
hardware/amlogic/stm/teseo/libteseo.utils/../include/teseo/utils/Signal.h:300:35: error: unused parameter 'args' [-Werror,-Wunused-parameter]
void logw(const char * fmt, T... args)
^
hardware/amlogic/stm/teseo/libteseo.utils/../include/teseo/utils/Signal.h:306:25: error: unused parameter 'fmt' [-Werror,-Wunused-parameter]
void loge(const char * fmt, T... args)
^
hardware/amlogic/stm/teseo/libteseo.utils/../include/teseo/utils/Signal.h:306:35: error: unused parameter 'args' [-Werror,-Wunused-parameter]
void loge(const char * fmt, T... args)
^
In file included from hardware/amlogic/stm/teseo/libteseo.utils/src/NmeaStream.cpp:28:
In file included from hardware/amlogic/stm/teseo/libteseo.utils/../include/teseo/utils/NmeaStream.h:38:
hardware/amlogic/stm/teseo/libteseo.utils/../include/teseo/utils/IByteStream.h:68:2: error: control reaches end of non-void function [-Werror,-Wreturn-type]
}
^
In file included from hardware/amlogic/stm/teseo/libteseo.utils/src/NmeaStream.cpp:28:
hardware/amlogic/stm/teseo/libteseo.utils/../include/teseo/utils/NmeaStream.h:48:2: error: direct base 'Trackable' is inaccessible due to ambiguity:
class stm::stream::NmeaStream -> class stm::stream::IStream -> class Trackable
class stm::stream::NmeaStream -> class Trackable [-Werror,-Winaccessible-base]
public Trackable
^~~~~~~~~~~~~~~~
hardware/amlogic/stm/teseo/libteseo.utils/../include/teseo/utils/NmeaStream.h:56:7: error: private field 'continueReading' is not used [-Werror,-Wunused-private-field]
bool continueReading;The link from ST to the library on GitHub says that there is support for Android 8+. I have Android 9 Pie. Apparently the source code from ST is old.
Hence the question, how can I get fresh sources for Teseo III? Or maybe someone has already remade libraries for Android9 or has experience embedding a driver in an Android system. I connect this module to Khadas VIM3 instead of SIM68, I want to upgrade to a more modern GNSS system
2020-04-26 10:58 PM
Hi
We are working to update the Teseo-HAL Android support.
It should be released End of Q2 2020.
Hope this helps
Regards
Francesco
2021-04-04 8:59 AM
Good day. Now the 1Q of 2021 is over. What news about the driver for Android 9+ is there?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.