2025-03-26 2:05 AM
I am working with the Teseo-LIV3F GNSS module, I would need to know whether the velocity field it produces, which is a module, is calculated over the x and y dimensions only or x,y and z
Thanks for your help
Solved! Go to Solution.
2025-04-09 10:31 AM - edited 2025-04-09 2:34 PM
Hi,
Could you please let me know which velocity field you are referring to?
If it is GGA it is a compound value of velocity in x,y and z.
However, you can enable either $PSTMPV or $PSTMPVRAW to see individual values of velocity in x,y and z dimensions.
This snipped of instruction below enables both PSTMPV and PSTMPVRAW. You can just select one of them.
$PSTMSETPAR,1228,0x1,1
$PSTMSETPAR,1228,0x4000,1
$PSTMSAVEPAR
$PSTMSRR
2025-04-09 10:31 AM - edited 2025-04-09 2:34 PM
Hi,
Could you please let me know which velocity field you are referring to?
If it is GGA it is a compound value of velocity in x,y and z.
However, you can enable either $PSTMPV or $PSTMPVRAW to see individual values of velocity in x,y and z dimensions.
This snipped of instruction below enables both PSTMPV and PSTMPVRAW. You can just select one of them.
$PSTMSETPAR,1228,0x1,1
$PSTMSETPAR,1228,0x4000,1
$PSTMSAVEPAR
$PSTMSRR
2025-05-14 4:39 AM - edited 2025-05-14 4:43 AM
My excuses for this delay, in the meantime we managed to find that message, we needed the PSTMPV one, which indeed delivers the velocity on 3 axes
2025-05-14 10:18 AM
Great ! Good to know that the problem has been resolved.
2026-02-10 12:51 PM
Hello,
I am trying to configure PSTMPV to output, but not succeeding. This is what I do:
I can check ID 200 with "$PSTMGETPAR,1200*20", and get back "$PSTMSETPAR,1200,0x09e7165c*5A". I don't see anything specifically in the software manual on those settings that control if I can enable PSTMPV, but I figured this could be important.
When I send "$PSTMNMEAREQUEST,00000062,00000001*49", I get back a single PSTMPV message, and my unit happens to have GPS lock.
However, when I try to enable PSTMPV to the current configuration with "$PSTMSETPAR,1228,0x1,1*76", I get back "$PSTMSETPAROK,1228*3A", but PSTMPV is not ever sent. When I request the setting with "$PSTMGETPAR,1228*2A", I get back "$PSTMSETPAR,1228,0x00024001*5D", which indicates that PSTMPV should be sent. However, I am still not seeing PSTMPV. Is there some other setting to set or check?
If relevant, I am using Teseo-Suite Pro NMEA decoding tool to view and send these commands.
Thanks!
2026-02-23 11:16 AM
Hi,
Can you please tell me which product you are using ?
$PSTMPV is available in LIV3F/LIV3FL.
Please refer to my earlier message in the thread of enable $PSTMPV.
Also in the software manual, you can refer to $PSTMSETPAR command to only set the required bits by using the bit mask.
2026-02-23 11:24 AM
I am using the TESEO-LIV3FL on a custom PCB.
I understand that it is supposed to support PSTMPV, and when I use the $PSTMNMEAREQUEST command, I get back a single PSTMPV message as a response.
My issue is that as far as I can tell the module is not working as expected. I think I am using the PSTMSETPAR command correctly, since when I send "$PSTMGETPAR,1228*2A", I get back "$PSTMSETPAR,1228,0x00024001*5D", which indicates that PSTMPV should be sent. However, I am not getting the PSTMPV message periodically. Are there any other settings that could impact this?
2026-02-23 11:52 AM
Are you getting all the standard NMEA messages that you have enabled?
What is GNSS update/output rate?
If you are outputting GNSS message at a higher rate > 1 Hz, please ensure that you are using a higher baud rate. Just wanted to ensure that that all UART messages are being received.
In addition, if you are enabling a lot of NMEA messages and outputting at higher rate, ensure that CDB-130 clock divider is set to 1.
You can use
$PSTMSETPAR,1130,0x0 //SET THE PARAMETER
$PSTMSAVEPAR //SAVE
$PSTMSRR //RESET for setting to take effect
I assume when you enable PSTMPV, you are saving and resetting the module.
2026-02-23 12:16 PM
Thank you! I had not used the save and reset commands:
$PSTMSAVEPAR
$PSTMSRR
Once I did those, I see PSTMPV output at 1Hz. Thank you for your help!
2026-03-05 12:12 PM
Can you confirm the direction of the "vertical velocity" field? If my altitude is increasing, will I get a positive number for vertical velocity?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.