2026-02-04 2:30 PM
Is there a way to turn the DC off on the RF_IN port on the LIV4 GPS module? There must be an enable or disable feature available via firmware. Thanks for reading.
Scott
2026-03-05 9:00 AM
Hi,
The capability to turn off DC bias in RF_IN line on LIV4F is not provided.
May I ask what is the use case for having this off? Is it trying to connect an active antenna with different input voltage?
2026-03-05 9:23 AM
2026-03-05 1:46 PM - edited 2026-03-06 7:04 AM
Ok, the RF signal chain is slightly different for LIV3F and LIV4F.
In this case you might have to put a blocking capacitor in front of LNA.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.