2024-11-16 11:25 PM
While upgrading Taseo Firmware for NavIC through UART interface to PC, I got the following error message:
Upgrade command error
Please check software baud rate or select recovery mode
My setting are:
Loader baud rate: 115200
Software baud rate 115200
Jumper settings
J6:2-3 (FW-UPG)
J7: 2-3(FW-UPG)
J11: NC
Request to confirm the correct baud rates or how to upgrade the firmware.
2024-11-17 12:02 AM
Check if both the loader baud rate and the software baud rate match, as they do in your settings (115200 in this case).
2024-11-17 9:18 AM
Thanks for your reply.
The problem is fixed now. Earlier, I was using 40 pin connector Rx and Tx pins which then I changed to J10 Rx and Tx.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.