| Subject | Author | Posted | |
|---|---|---|---|
|
We are interfacing the IMP34DT05TR microphone with the STM32F423ZHJ6 microcontroller. I have attach...
| 2025-03-26 11:38 PM | ||
|
Hello friends; I aim to develop FreeRTOS STM32 based flight control card software. First of all, I...
| 2025-03-23 4:24 AM | ||
|
It seems that its CS is inactive, the LIS will assume that it should be in I2C mode. But if I have...
| 2025-03-12 11:14 AM | ||
|
Hello, I'm looking for any available douments/application notes on how to mount the sensor on a de...
| 2025-03-12 6:30 AM | ||
|
We have a ILPS22QS pressure sensor. We are getting an occasional i2c error. On investigation it s...
| 2025-03-12 12:45 AM | ||
|
I have an LSM6DSV16X configured to generate an interrupt on INT1 whenever the FIFO contains more el...
| 2025-02-25 5:58 AM | ||
|
Issue with Wrist Tilt Direction Detection on LSM6DS3TR-C Hardware & Software Details: - Sensor: L...
| 2025-02-23 10:52 PM | ||
|
Hi We are currently working on a project using the nRF5340 MCU with Zephyr, and the interface betw...
| 2025-02-19 2:33 AM | ||
|
Dear ST/Forum, Preamble: We are using the LPS22HBTR pressure-temperature sensor in some PCB assem...
| 2025-02-05 4:58 AM | ||
|
I have a LIS3MDLTR connected over I2C on an aerial system that is used as part of our GNC system. ...
| 2025-01-29 6:25 AM | ||
|
Hi everyone, We are using the STEVAL-STWINKT1B board as a reference for the study of condition mon...
| 2025-01-16 12:12 AM | ||
|
We have an issue with LSM6DSM and LSM6DSV. Sometimes they start consuming abnormally high current o...
| 2025-01-06 12:04 PM | ||
|
HI When using the FIFO mode on the lsm6ds3tr-c sensor, there appears to be an issue where occasion...
| 2024-12-26 8:03 PM | ||
|
Hi Everyone, I'm using STM32L4 with LSM6DSM on IAR IDE and using motion AC library to calibrate th...
| 2024-11-29 5:22 AM | ||
|
Hello, We have implemented the LIS3DH with a nRF52832 in I2C mode on our board, and are using the ...
| 2024-11-27 12:18 PM | ||
|
Does the IIS2MDC require burn-in? Using the IIS2MDC, I read a magnetic filed of 0.47 Gauss on a Fri...
| 2024-11-12 8:20 AM | ||
|
I BOUGHT STEVAL- MKBOX PRO AND AM THINKING OF USING IT.
I have a wireless function, but pleas...
| 2024-11-10 6:57 PM | ||
|
After programming bluenrgm2sp module it is not discoverable in the ST BLE-scanner.I have used the b...
| 2024-10-27 10:39 PM | ||
|
I am using NRF5340 board for development using the LSM6DSO IMU sensor. Is there any way so that I ...
| 2024-10-26 8:52 PM | ||
|
Back in 2015, I ordered 19 LSM9DS0 boards from Adafruit for a project (which is taking longer tha...
| 2024-10-25 2:38 AM |