| Subject | Author | Posted | |
|---|---|---|---|
|
I am using the STHS34PF80 sensor (SparkFun Presence Sensor - STHS34PF80) with an ESP32 in my ceilin...
| 2025-08-17 11:35 PM | ||
|
Hello, I'm working on an IMU project. I need to measure pitch/roll/yaw rotation in quaternions. F...
| 2025-08-11 5:24 AM | ||
|
Hi, I’m using the NUCLEO-STM32F401RE with the X-NUCLEO-CCA02M2 board, which has two MP34DT06 PDM m...
| 2025-08-06 12:20 AM | ||
|
Hi ST guys, I played with the LIS3DH accelerometer options and don't really see difference in inte...
| 2025-07-31 8:04 AM | ||
|
Hi, I am follow up on the query i am posted "https://community.st.com/t5/mems-sensors/integratin...
| 2025-07-29 10:35 PM | ||
|
Hi, I am using LSM6DSO as my I3C sensor. It works well with RSTDAA and ENTAA. But when I tried to g...
| 2025-07-29 2:01 AM | ||
|
Dear all, I am using SensorTile.box STEVAL-MKSBOX1V1 with St app. I made application with vibrome...
| 2025-07-25 2:09 AM | ||
|
dear all, i want to recoed acceleration date from LSM6DSOX . i made app on st app and made output...
| 2025-07-23 9:15 AM | ||
|
Hi, I have a compulab SBC (UCMiMX8Mplus sbev) it is a dev kit. I am connecting the STEVAL-55GMB...
| 2025-07-17 7:48 AM | ||
|
I'm currently working with the LSM6DSV16X IMU and would like to connect an external sensor—specific...
| 2025-06-30 2:10 PM | ||
|
Hi, I am working on an accelerometer interrupt using the LSM6DSM. In AN4987 I found that I can con...
| 2025-06-27 12:23 AM | ||
|
I need to implement the clock wise motion using the sensor like LIS3DH accelerometer with i2c prot...
| 2025-06-24 4:33 AM | ||
|
I have implemented 9D orientation calculation on the STM32L4 using the LSM6DSO16IS and LIS2MDL sens...
| 2025-06-12 6:14 AM | ||
|
Hi everyone, I have set up my LIS2DW12 to recognise double taps in the Z direction, which works we...
| 2025-06-04 7:24 AM | ||
|
Hello everyone, I am using the LIS2MDL sensor in a parking project, where it operates via interrup...
| 2025-05-23 7:07 AM | ||
|
Hi, First of all, I'm not proficient with embedded C, but I would appreciate any input from you...
| 2025-05-19 10:36 PM | ||
|
Hello STM32 Community, I'm working with the LSM303AGR magnetometer/accelerometer sensor on an S...
| 2025-05-11 9:40 PM | ||
|
We've implemented an example program based on UM2220 using an lsm6dsox IMU sensor on an STM32U575 m...
| 2025-05-08 8:07 AM | ||
|
Has anyone tested the LIS2DE12TR accelerometer using lower input capacitance? I am interested in tr...
| 2025-04-30 11:27 AM | ||
|
Hi ST Community, I’m trying to use the LSM6DSO32XTR in Mode 2 (SensorHub) to stream data from two ...
| 2025-04-28 2:07 AM |