| Subject | Author | Posted | |
|---|---|---|---|
|
Hi all I have used CubeMx to create an FMC interface to psram(nonmultiplex) 8-bit data 10-bit addr...
| 2024-10-13 11:53 PM | ||
|
I have created a CPP critical section class using stm32_lock_acquire and stm32_lock_release. The m...
| 2024-10-09 8:09 AM | ||
|
Hi, Please see attached video: This is a image based slider in LVGL, with nothing going on exc...
| 2024-10-02 7:15 AM | ||
|
STM32Cube FW_H7 V1.11.2 I previously posted an issue related to incorrect selection of the interna...
| 2024-09-25 8:39 AM | ||
|
Hello, I'm debugging the following piece of code that is executed as part of the fault handler: c...
| 2024-09-18 7:17 AM | ||
|
Hello I am Working with EC200U & STM32F411CEU6. I want to uplode code using AWS/cloud or hostinger ...
| 2024-09-14 2:29 AM | ||
|
Issue: Receiving NACK During STM32G0B1KEU6 Page Erase over I²C in Bootloader Mode Context: I am w...
| 2024-09-10 10:50 AM | ||
|
I have been examining the X-CUBE-EEPRMA1 codebase and noticed a couple of issues with the code that...
| 2024-07-25 8:54 AM | ||
|
I'm using STM32U073MCT6 MCU. I have a custom board (which contains this MCU and other required comp...
| 2024-07-23 6:07 AM | ||
|
Hello, I am trying to send and receive data with LoRa using STM32. I will leave the codes below. Th...
| 2024-07-15 1:00 PM | ||
|
stm32h7xx_hal_uart.c is missing a prompt to enable usart interrupt in the DMA configuration instruc...
| 2024-07-11 9:36 PM | ||
|
During audio codec processing, I encountered errors such as "UnboundLocalError: local variable 'res...
| 2024-07-10 8:33 PM | ||
|
So I am using STMG030F6P6TR to play raw audio stored in SPI flash using PT8211 DAC and LM4890S ampl...
| 2024-07-04 2:29 AM | ||
|
Hi everyone! I was hoping to get some help on a function I've made which is called by timer to writ...
| 2024-06-28 3:49 PM | ||
|
Hello Community, I am encountering an error after my STM32H7ZIT6 device runs for a few hours. Th...
| 2024-06-21 9:38 PM | ||
|
Hello, I am using the nucleo h755zi-q board on my project. I am having issues with getting the uar...
| 2024-06-19 11:39 AM | ||
|
Is it possible to make HAL_ADCEx_EndOfSamplingCallback fire when ADC is running in the dual mode wi...
| 2024-06-17 7:17 AM | ||
|
We will be submitting our STM32F101vft based appliance for UL certification. We found the self-tes...
| 2024-06-12 8:25 AM | ||
|
I am using a Nucleo-u083rc to run the ADC_MultiChannelSingleConversion Application from STM32Cube M...
| 2024-06-12 12:34 AM | ||
|
Dear Team, I hope this email finds you well. I am reaching out to discuss a technical challenge we...
| 2024-06-09 11:35 PM |