| Subject | Author | Posted | |
|---|---|---|---|
|
Hello,
First of all, NetXDuo is working fine on the NUCLEO-H743ZI board. (PING, UDP, TCP)
E...
| 2025-02-25 1:54 AM | ||
|
Hi all,
I am using a STM32H747XIH6 MCU.
I developed an application using LwIP library.
When I...
| 2025-02-17 8:39 PM | ||
|
I have an optimized SPI Slave DMA setup which is driven by the chip select interrupt. It looks some...
| 2025-02-05 7:24 AM | ||
|
My goal is to display text on the TFT LCD using stm32F756. The display I have is just the screen, n...
| 2025-02-04 6:48 PM | ||
|
I don't know if libopencm3 code is allowed to post here but really isn't that different at all... ...
| 2025-01-27 4:12 PM | ||
|
Currently using STM32L4R9I-Discovery.
I want to pass an entire buffer to a sd card using idma sdm...
| 2025-01-22 1:56 AM | ||
|
Guys, it was really hard giving birth to this proof of concept: - Every 100ms the timer hits the ...
| 2025-01-16 7:04 AM | ||
|
Hello Forum,
I have a question regarding OTA and toggling between flash banks on a STM32L496....
| 2025-01-13 8:28 AM | ||
|
Hi, I'm trying to use https://www.st.com/en/embedded-software/x-cube-eeprom.html on my custom stm32...
| 2024-12-29 2:53 PM | ||
|
Good morning everyone, I'm here to ask for advice regarding the approach I want to take for enabli...
| 2024-12-23 12:38 AM | ||
|
Hello Everyone, I am working on a UVC project using the STM32U5G9ZJT6Q MCU, capturing 8-bit data v...
| 2024-12-17 1:27 AM | ||
|
Hello I'm developing RTOS environment of dual-core in STM32H757. Using the functions osThre...
| 2024-12-16 9:29 PM | ||
|
Hello STM Community!, I'm trying to implement USB CDC ACM in standalone mode(without using ThreadX...
| 2024-12-16 3:39 AM | ||
|
I recently began using the B-L462E-CELL1 module for IoT applications, connecting it to a Raspberry ...
| 2024-12-15 11:27 PM | ||
|
hi, im using stm32g474vet6 tim_bkin for pwm shutdown through external pin, when im normally using p...
| 2024-12-11 6:15 PM | ||
|
Hi everyone, I encountered a challenging issue while using GUIDRV_LIN_OSY_16 with STemWin on an ST...
| 2024-12-11 4:21 AM | ||
|
Hello, I am newbie and i have project with STM32F407G-DISC1 and PMOD I2S2. It generates two RNG va...
| 2024-12-07 8:56 AM | ||
|
Hi, I have an http web server running on a STM32U575. The system is reachable via USB over RNDIS. H...
| 2024-12-06 11:26 PM | ||
|
Dear all !
I in my project have 1 led was blink to know CPU still working, display TFT LCD ST7735...
| 2024-12-04 10:26 PM | ||
|
I am using a user defined diskio function (found online here https://github.com/kiwih/cubeide-sd-ca...
| 2024-12-02 7:01 PM |