| Subject | Author | Posted | |
|---|---|---|---|
|
FreeRTOS is not started, failed on configASSERT( ( portMAX_PRIGROUP_BITS - ulMaxPRIGROUPValue ) == ...
| 2024-12-02 4:10 AM | ||
|
Hi
Is there a plan to update the x-cube-freertos Kernel to 11.1.0?
Github repo: STMicroelectron...
| 2024-12-01 11:15 PM | ||
|
Hello ST Community, I’m working on a project where I initially developed software on the STM32H735...
| 2024-11-25 2:41 AM | ||
|
Good afternoon, We use ThreadX in conjunction with TouchGFX. As debugger we use ST-Link/V2...
| 2024-11-24 10:44 PM | ||
|
Hello, trying to port Miro Samek's example: https://github.com/QuantumLeaps/FreeACT - into my n...
| 2024-11-24 3:26 PM | ||
|
Hi, my goal was to play some .wav audio files from an external SD card using the onboard DAC and an...
| 2024-11-23 5:02 PM | ||
|
Hi All I have a problem with a ThreadX-based project on a Nucleo H563ZI board when using a mutex. ...
| 2024-11-20 9:28 AM | ||
|
Hi,
I have a custom PCB where I am attempting to bootload an STM32G071CBU6 (using an STM32U575). ...
| 2024-11-14 7:16 PM | ||
|
Hello everyone and thank you for your help, I am being using the STM32F746G-Discovery Board for a c...
| 2024-11-10 11:14 PM | ||
|
Hi, I would like to know if I can emulate the STM32H5 (which is ARM cortex-M33) via Qemu. And if s...
| 2024-11-10 6:00 PM | ||
|
Hi, my stm32f103 freeze after osKernelStart() after jump from bootloader but if I flash at that add...
| 2024-11-07 11:24 PM | ||
|
I am writing an embedded software project that includes BLE GATT protocol with stm32wb15 mcu. Base...
| 2024-11-05 2:43 AM | ||
|
Hello Together, I have an issue regarding my STM32 Project I tried different things and do not ge...
| 2024-11-04 5:51 AM | ||
|
Good evening, I would be interested in getting more information about the BLEMLC Firmware for the S...
| 2024-11-02 8:40 AM | ||
|
Tôi đã triển khai thành công việc truyền dữ liệu giữa STM32 NUCLEO F429ZI của mình và một broker MQ...
| 2024-10-30 2:06 AM | ||
|
Hello I'm developing RTOS environment of dual-core in STM32H757. I could refer to the examples...
| 2024-10-29 7:22 PM | ||
|
I want to create two nodes program, one node has two publishers and the other one handles a service...
| 2024-10-24 7:37 AM | ||
|
Hello everyone! I am contacting you because I have not succeeded in creating an executable e...
| 2024-10-23 2:01 AM | ||
|
The update function using the DUALBANK SWAP function added to the firmware for the old CPU (STM32L4...
| 2024-10-22 9:53 PM | ||
|
Hi, I am using STM32CubeIDE and an ST-LINK V2 to program a custom board that runs off an STM32WB10...
| 2024-10-21 12:33 AM |