| Subject | Author | Posted | |
|---|---|---|---|
|
Hello! This is the first time im using NOR Flash so bear with me :) Question #1 I screwed up an...
| 2024-10-31 3:08 AM | ||
|
Hi I am using X-CUBE-DPOWER to set the parameters for my Buck converter operating conditions on a...
| 2024-10-30 10:17 PM | ||
|
This is a problem about the STM32H745XI-Disco control external AD5791 through SPI. When using Debug...
| 2024-10-30 6:46 AM | ||
|
I am working on the development of a Bootloader for one of our projects. We are encountering an iss...
| 2024-10-27 11:40 PM | ||
|
Hello. Is there an example F/W for STEVAL-ESC001V1 or X-NUCLEO-IHM08M1 that is SPL compatible? I ...
| 2024-10-27 7:35 PM | ||
|
Dear STM Community I am reaching out on behalf of our development team, as we are in the process o...
| 2024-10-27 1:22 AM | ||
|
I'm trying to program an STM32U5 microcontroller with Open On-Chip Debugger 0.12.0+dev-00597-ga5a21...
| 2024-10-26 8:19 AM | ||
|
Hello, I'm trying communication between stm32G0 as I2C slave and a rapsberry pi 5 as master. o...
| 2024-10-25 2:31 AM | ||
|
I'm working on a STM32G473RCT6 CPU with 256K Flash in dualbank mode. looking for information on ad...
| 2024-10-24 7:20 AM | ||
|
For my current project, I am seeking recommendations for the most suitable STM32 microcontroller se...
| 2024-10-22 10:10 PM | ||
|
I’m new to the STM32L4 community and currently working on an assignment for my studies, using the S...
| 2024-10-21 12:22 PM | ||
|
Hi, the device have some kind of limitation on the usage of DMA? What I did: 1 - Implemented DMA0...
| 2024-10-20 11:46 PM | ||
|
I have an STM32F103VET6 with multiple DMA Channels like UART2_RX, ADC, UART3_RX, UART3_TX, all at d...
| 2024-10-20 10:35 PM | ||
|
Hello I'm developing RTOS environment of dual-core in STM32H757. In OpenAMP communication mode...
| 2024-10-20 7:18 PM | ||
|
Hi. First time using this forum. I'm using an STM32F103C8 (genuine, not bluepill clone). I've eas...
| 2024-10-20 3:31 AM | ||
|
Hi everyone! I have this code where the mcu goes into STOP3 mode, and is waked up by a button trig...
| 2024-10-14 3:22 PM | ||
|
Dear Team, We are using the STM32G473VET6 microcontroller with the IMP34DT05TR microphone, uti...
| 2024-10-10 6:28 AM | ||
|
I redid FatFS to work async or in polling mode. Works well on my STM32H755zi, on CM4. Most function...
| 2024-10-09 8:04 AM | ||
|
Hello, I am trying to integrate internet connectivity on the STM32F407 using an LTE modem via the ...
| 2024-10-08 8:37 AM | ||
|
Hi. I am using the STM32H7S78-DK board. In STM32CubeIDE, I checked the example for jpeg_encodi...
| 2024-10-02 12:19 AM |