| Subject | Author | Posted | |
|---|---|---|---|
|
Hello,
we use STM32F413RGT6 as slave board communicate through rs485 bus. In application, we driv...
| 2025-07-28 7:27 AM | ||
|
Moved from this thread.
What is the maximum amount of time required after bringing nRST high for ...
| 2025-07-09 8:17 AM | ||
|
I'm writing a small HAL of my own for the STM32F1 and I noticed that sometimes the DMA would read i...
| 2025-06-09 6:18 PM | ||
|
Hello. I work on a project (the microcontroller is STM32H733VGT6) where VBAT mode is used. When th...
| 2025-06-03 3:36 AM | ||
|
I'm working on a project which uses DMA to pull data from an external chip controlled by the FMC in...
| 2025-05-29 1:25 PM | ||
|
Hello, I am using STM32F030C8T6 to implement Modbus RTU protocol which uses UART and RS485 as phys...
| 2025-05-23 1:07 PM | ||
|
Board: NUCLEO-H723ZG MCU: STM32H723ZG (applies to others as well) Reference manual: RM0468 Rev. 3...
| 2025-05-21 12:56 AM | ||
|
Hi, I have an STM32F407-DISC1 connected to an Raspberry PI via I2S. The clock frequency is about 3M...
| 2025-05-20 1:42 AM | ||
|
Hi I'm planning to make a digital mixer that takes 4 analog audio input channels (2x stereo), proc...
| 2025-04-29 5:37 AM | ||
|
I'm working on recording audio synchronously using multiple I2S microphones connected to different ...
| 2025-04-23 3:57 AM | ||
|
Hello, I am working on a simple project at STM32L476 NUCLEO which includes ADC1 + TIM6 + DMA1. No ...
| 2025-04-09 1:25 PM | ||
|
Moved from Feedback Forum.
The Feedback Forum is not for product questions.
Hello ev...
| 2025-04-03 1:47 AM | ||
|
Hello, I am working with the STM32H503CBT6 and using the I3C Transmit_IT in Controller mode for co...
| 2025-03-28 12:46 AM | ||
|
Hi, Anyone can help with resources (videos, Documents), to understand how to calculate time dela...
| 2025-03-10 9:40 PM | ||
|
I'm trying to use a STM32 Nucleo-L476RG to get audio from a PDM MEMs Microphone (Infineon IM66D120A...
| 2025-03-10 12:02 PM | ||
|
Hello, I am trying to write to the option byte area of an stm32u5g9vjt6q using the built in bootloa...
| 2025-02-23 12:53 PM | ||
|
Hello, I have a NUCLEO U545 - REQ and i have a Queue in which i read the incoming values from ...
| 2025-02-21 2:25 AM | ||
|
Can anyone comment on the prologue and epilogue of following CM7 code, particularly the content of ...
| 2025-02-03 5:37 AM | ||
|
Howdy, I am currently working with a STM32U575 and currently having a problem with the ADF. I am t...
| 2025-01-27 9:29 AM | ||
|
Hi everyone, I’m working on a custom board design using an STM32H753AII6 in the UFBGA169 package. ...
| 2025-01-23 2:03 AM |