| Subject | Author | Posted | |
|---|---|---|---|
|
Hello, I am considering the STM32H7 for a new project I'm working on. I'd like to configure the M...
| 2025-01-16 2:39 PM | ||
|
I am trying LTDC color keying application. LTDC uses HSI as clock source. I want to make all system...
| 2024-12-30 9:06 AM | ||
|
Hello everyone, why is it that the ITM output does not display when the IDE jumps from boot to Appl...
| 2024-12-30 12:52 AM | ||
|
Hello everyone I need to implement a protocol for an external ADC. An SPI read with 22 bits should...
| 2024-12-18 2:05 AM | ||
|
Dear community, It is now public and available at distributors : https://www.st.com/stm32n6
| 2024-12-17 12:48 AM | ||
|
I am trying to read the data interpreted in a SIF signal using a Nucleo-F072RB. There are three p...
| 2024-12-11 8:02 PM | ||
|
This code, partially generated by Copilot, does only print "=" At the same time, I do see that the...
| 2024-12-10 10:09 AM | ||
|
In STM32H735IGT mcu I have initialized ADC1 and ADC3 in DMA method, also FreeRTOS is initialized. B...
| 2024-12-10 3:17 AM | ||
|
I am experiencing an issue with the STM32 microcontroller used in a Battery Management System (BMS)...
| 2024-12-09 9:34 PM | ||
|
Hello, I use STM32F407G-DISC1 with Digilent PMOD I2S2. I have FIR filter project and after i enabl...
| 2024-12-09 10:07 AM | ||
|
Hello folks!
One of my devices happened to have a some kind of flash corruption, enough that an E...
| 2024-12-05 12:10 AM | ||
|
I am useing ADC with STM32H743ZIT6 device.when i debugging,i find that the device can't read DBGMCU...
| 2024-11-29 7:44 AM | ||
|
Hi, I am trying to do synchronous DAC and ADC sampling using timers on the STM32H747. A simplifie...
| 2024-11-29 6:53 AM | ||
|
Hello there! I would like to ask for help from those who know this MCU family about the system mem...
| 2024-11-28 1:43 AM | ||
|
I've been able to get the higher frequency to output on the tamper pin but not the seconds pulse. ...
| 2024-11-27 2:06 AM | ||
|
Hi, We apply the single-end analog inputs to STM32H753ADC 1, 2, 3 respectively. .1. ADC 1, 2...
| 2024-11-25 4:32 PM | ||
|
GOAL: Currently I am trying to get to know the low power capabilities with the STM32H757I-Eval Boa...
| 2024-11-25 3:48 AM | ||
|
Good morning to all, I was wanting to save data in the non volatile memory of my STM32H745i-Disk w...
| 2024-11-23 8:03 PM | ||
|
Hello, I am implementing my own I2C drivers based on the LL drivers provided by stm32g031xxxx (STM...
| 2024-11-23 7:29 PM | ||
|
Hello, I am programming STM32G491, while I need to use nRST as GPIO (MCO). I am using a code that ...
| 2024-11-23 3:31 PM |