2024-02-09 7:55 AM - edited 2024-02-10 12:31 AM
This is something I haven't seen in last couple of months, but appeared and happens relatively often since last week or two.
#updates_are_not_universally_good_thing
#unnecessary_javascriptoiding_is_a_bad_thing
JW
2024-04-15 2:44 AM - edited 2024-04-15 2:49 AM
@Andrew Neil wrote:After using any other 'Reply' button in the thread, that one does seem to remember what it's supposed to do.
Actually, it seems that the yellow one is "dimmed":
It has let me click in the box, and the box border has gone bold - so it's recognised my click, and set the focus - but it doesn't present the composition window, and doesn't allow me to type anything. It doesn't even give a caret in the box.
But If I click on the blue 'Reply' button, I get two composition windows!
First is the one for the blue reply button to the specific post; second is the one for the yellow button
EDIT
@waclawek.jan did mention the two-window thing earlier.
NXP seem to be using the same forum software. On there, they have a "quick reply" which, IIRC, doesn't present a full composition window - it's just a quick "type in the box".
Maybe this forum is trying to do that, but failing?
2024-04-15 7:34 AM
Hello all,
Thank you for your reports on this issue.
After investigation, it has been identified as a bug. I will update you once I have more information to share about the fix.
I am sorry for this inconvenience,
Lina
2025-03-18 3:28 AM
Hello all,
This issue has been fixed. Let us know if you still face it on your end.
Thank you,
Lina
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.