cancel
Showing results for 
Search instead for 
Did you mean: 

Pasting images not working

Andrew Neil
Super User

For the past week or so, pasting images directly into posts seems to have broken.

I used to be able to just take a screenshot, or copy an image and paste it straight into the editor, but that no longer works.

I press 'paste', and nothing happens - no error messages or anything.

I am now having to save the image locally, and then use the 'Insert Photos' button to import it.

 

There is history with this, but now it seems to have just broken completely.

 

Using Chrome Version 145.0.7632.109 (Official Build) (64-bit) on Windows-11 Pro

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi @Andrew Neil.

Yes, this has been fixed this morning as well. I am happy to see it's working for you! 

Lina


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

14 REPLIES 14
TDK
Super User

Same experience here. Edge browser. Was wondering if it was just me.

If you feel a post has answered your question, please click "Accept as Solution".
AScha.3
Super User

+ same on Chrome / Linux .

If you feel a post has answered your question, please click "Accept as Solution".
Maxime_MARCHETTO1
Community manager

Thank you for sharing your feedback.

We are aware of this issue and are currently working with our platform provider to resolve it. Unfortunately, we do not have a timeline to share at the moment.

Thank you for your understanding,
Maxime

 

TDK
Super User

Probably related to this, I have 3 times now had only part of my post go through. The rest of my post is lost and I have to retype it. The part that is lost start at an image I include.

I'm not losing my mind. There's no way I would only post a one word sentence response here:

ST-Link error - STMicroelectronics Community

 

Edit: the screenshot I put in this post disappeared when I hit the yellow "Reply" button.

If you feel a post has answered your question, please click "Accept as Solution".

I think I just had this happen.

I hadn't seen it happen before, so looks like a new issue?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Maxime_MARCHETTO1
Community manager

Thank you for sharing additional information. The software provider has been informed of this new issue and is currently working on a fix. We hope to have it resolved soon.

TDK
Super User

Hey this is still happening.

If you feel a post has answered your question, please click "Accept as Solution".

Indeed, @TDK , the fix has not yet been implemented. We will inform once it's done. For the time being, please use the other existing option: 

1. Picture upload in the text editor: 

 

Screenshot 2026-03-04 155948.png

 

Regards,
Lina


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

@Lina_DABASINSKAITE wrote:

1. Picture upload in the text editor: 


@TDK @AScha.3 also dragging & dropping still works.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.