2025-03-21
8:24 AM
- last edited on
2025-03-24
3:32 AM
by
Lina_DABASINSKA
But quoting with code blocks is still broken.
Reply moved from this thread: Don't litter posts with whitespace (empty paragraphs inserted around code blocks)
2025-03-21 8:47 AM
@Andrew Neil wrote:But quoting with code blocks is still broken.
Indeed.
Composing a post with a quote with a code block inside:
Trying to post:
Final post:
2025-03-21 9:45 AM
Yes - that's the one!
I thought I had a thread about that, but can't find it.
2025-06-21 1:37 AM - edited 2025-06-21 1:38 AM
The editor shows it OK:
the code is within the quote block
But posting breaks it:
the code is now outside the quote block
When this happens, you get the "Invalid HTM was found" message.
So it seems that the problem is in whatever it is which performs this HTML "check" ?
2025-06-26 1:57 AM - edited 2025-06-26 3:08 AM
Hi Andrew,
Thanks for reporting, I could replicate the issue.
However, in the scenario when the code was simply copied/pasted in the quote and not embedded via the Insert/Edit code sample, the publication went through and code stayed in the same quote block (the error was still received, but double-clicking on it did the job).
Let me bring this issue further with the support team and I’ll get back to you.
If you notice anything else, let us know.
Thanks,
Lina
2025-06-26 2:00 AM
@Lina_DABASINSKAITE wrote:(the error was still received, but double-clicking on it did the job).
Yes, that error comes up a lot - usually for no apparent reason.
Usually, just hitting 'Post' again works - with no obvious changes!
2025-06-30 3:35 AM
Hello all,
The support team has successfully replicated the issue and confirmed that it's a bug. The engineering team is actively working on a resolution. At this time, we can go give any estimation of when it will be solved.
I will keep you posted once it's done.
Regards,
Lina
2025-06-30 3:43 AM
@Lina_DABASINSKAITE wrote:The support team has successfully replicated the issue and confirmed that it's a bug.
Is that the issue with the quoting, or the issue with the frequent "Invalid HTML" messages?
2025-06-30 5:34 AM
i also face this issue, when i copy pasted improvised post from chatGPT, i was thing its a feature that autmatically removes HTML codes insterted by chatGPT.
2025-06-30 6:44 AM
@jumman_JHINGA wrote:i also face this issue,
Which issue?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.