2025-03-18 4:06 AM
I am a newbie with STM32N6570-DK.
My target is to deploy AI model on this board. Which software do I need to install to start with STM32N6570-DK? I means that all softwares.
Thank you.
Solved! Go to Solution.
2025-03-18 7:03 AM
Hello @Anhem ,
I would suggest you start with ST Model Zoo:
STMicroelectronics/stm32ai-modelzoo: AI Model Zoo for STM32 devices
This github repository is composed of 2 parts:
Make sure to follow the before you start in ST Model Zoo Services (at the end) to install everything correctly.
Also, to deploy model on N6, follow this document (example for object detection). You will need to download a few additional things:
Have a good day,
Julian
2025-03-18 4:29 AM
https://www.st.com/en/evaluation-tools/stm32n6570-dk.html#tools-software
2025-03-18 7:03 AM
Hello @Anhem ,
I would suggest you start with ST Model Zoo:
STMicroelectronics/stm32ai-modelzoo: AI Model Zoo for STM32 devices
This github repository is composed of 2 parts:
Make sure to follow the before you start in ST Model Zoo Services (at the end) to install everything correctly.
Also, to deploy model on N6, follow this document (example for object detection). You will need to download a few additional things:
Have a good day,
Julian
2025-03-19 2:46 AM
Hi @Julian E.
Thank you. I am following with this link.
Step 1: I installed STM32CubeIDE and installed STEdgeAI (for generating C code from tflite/onnx).
Step 2: I also downloaded STM32N6 Getting Started V1.0.0 and copy application_code to modezoo-services https://github.com/STMicroelectronics/stm32ai-modelzoo-services/blob/main/application_code/object_detection/STM32N6/README_ModelZoo.md
I have a question. Whether I need to instal CubeMX and install X-CUBE-AI in CubeMX.
As my understanding with STEdgeAI we can generated C code from tflite/onnx, why we need X-CUBE-AI more?
Moreover, I tried installed CubeMX and X-CUBE-AI inside CubeMX, it seems that I need to download STEdgeAI again and NPU Art inside CubeMX. This made me confuse because in the aboe step 1, we have already installed STEdgeAI and NPU Art.
2025-03-19 2:59 AM - edited 2025-03-19 3:00 AM
Hello @Anhem ,
Sure, it is a little bit hard to understand.
CubeMX is useful to generate project when starting from zero.
The application codes were started using cubeMX.
In your case, you will use the application code, so you don't need it. In the future, if you want to start your project from blank, you will need it to configure the I/O, get the LL and HAL libraries etc.
For X Cube AI, I would explain it as a GUI in CubeMX for ST Edge AI core.
So if you were to add manually an AI model in a new project, the easiest way would be to use X Cube AI for it to generate all your c files and generate a CubeIDE project with a template code.
You could use ST Edge AI, get your files, and manually add it to your project folder and add the path in CubeIDE for the builder to find your files.
With model zoo, it is the deployment script that will call st edge ai, get your model as c files and replace it automatically in the application codes.
To sum up, st edge ai core is the heart of everything, it is the software that does the conversion.
Most of the AI tool are way to use it: ST Dev cloud uses it in background, X Cube AI also and Model Zoo scripts
So, for now, you have installed everything that you need.
Have a good day,
Julian
2025-03-19 7:29 PM
Hi @Julian E.
It is more clear for me. I want to understand about this point
Moreover, I tried installed CubeMX and X-CUBE-AI inside CubeMX, it seems that I need to download STEdgeAI again and NPU Art inside CubeMX.
It means that STEdgeAI and NPU ART that I installed outside CubeMX is seperated with STEdgeAI and NPU ART in CubeMX. Is that right? STEdgeAI and NPU ART in CubeMX are used only when we use CubeMX. Is that right?
Thank you.
2025-03-19 11:59 PM
Hi @Julian E.
I follow this link https://github.com/STMicroelectronics/stm32ai-modelzoo-services/blob/main/object_detection/deployment/README_STM32N6.md and I got this error.
My PC do not have GPU so I commented out some code in stm32ai.py
2025-03-20 13:56:14.310314: W tensorflow/stream_executor/platform/default/dso_loader.cc:64] Could not load dynamic library 'libcudart.so.11.0'; dlerror: libcudart.so.11.0: cannot open shared object file: No such file or directory
2025-03-20 13:56:14.310329: I tensorflow/stream_executor/cuda/cudart_stub.cc:29] Ignore above cudart dlerror if you do not have a GPU set up on your machine.
[INFO] : Running `deployment` operation mode
2025/03/20 13:56:16 INFO mlflow.tracking.fluent: Experiment with name '<unnamed>' does not exist. Creating a new experiment.
[INFO] : ClearML config check
[INFO] : The random seed for this simulation is 123
INFO: Created TensorFlow Lite XNNPACK delegate for CPU.
[INFO] : Generating C header file for Getting Started...
[INFO] : This TFLITE model doesnt contain a post-processing layer
loading model.. model_path="../../stm32ai-modelzoo/object_detection/ssd_mobilenet_v2_fpnlite/ST_pretrainedmodel_public_dataset/coco_2017_person/ssd_mobilenet_v2_fpnlite_035_192/ssd_mobilenet_v2_fpnlite_035_192_int8.tflite"
loading conf file.. "../../application_code/object_detection/STM32N6/stmaic_STM32N6570-DK.conf" config="None"
"n6 release" configuration is used
[INFO] : Selected board : "STM32N6570-DK Getting Started Object Detection (STM32CubeIDE)" (stm32_cube_ide/n6 release/stm32n6)
[INFO] : Compiling the model and generating optimized C code + Lib/Inc files: ../../stm32ai-modelzoo/object_detection/ssd_mobilenet_v2_fpnlite/ST_pretrainedmodel_public_dataset/coco_2017_person/ssd_mobilenet_v2_fpnlite_035_192/ssd_mobilenet_v2_fpnlite_035_192_int8.tflite
setting STM.AI tools.. root_dir="", req_version=""
Cube AI Path: "/opt/ST/STEdgeAI/2.0/Utilities/linux/stedgeai".
[INFO] : Offline CubeAI used; Selected tools: 10.0.0 (x-cube-ai pack)
loading conf file.. "../../application_code/object_detection/STM32N6/stmaic_STM32N6570-DK.conf" config="None"
"n6 release" configuration is used
compiling... "ssd_mobilenet_v2_fpnlite_035_192_int8_tflite" session
model_path : ['../../stm32ai-modelzoo/object_detection/ssd_mobilenet_v2_fpnlite/ST_pretrainedmodel_public_dataset/coco_2017_person/ssd_mobilenet_v2_fpnlite_035_192/ssd_mobilenet_v2_fpnlite_035_192_int8.tflite']
tools : 10.0.0 (x-cube-ai pack)
target : "STM32N6570-DK Getting Started Object Detection (STM32CubeIDE)" (stm32_cube_ide/n6 release/stm32n6)
options : --st-neural-art default@../../application_code/object_detection/STM32N6/Model/user_neuralart.json --input-data-type uint8 --inputs-ch-position chlast
[returned code = 255 - FAILED]
$ cwd: None
$ args: /opt/ST/STEdgeAI/2.0/Utilities/linux/stedgeai generate --target stm32n6 -m ../../stm32ai-modelzoo/object_detection/ssd_mobilenet_v2_fpnlite/ST_pretrainedmodel_public_dataset/coco_2017_person/ssd_mobilenet_v2_fpnlite_035_192/ssd_mobilenet_v2_fpnlite_035_192_int8.tflite --output /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/experiments_outputs/2025_03_20_13_56_16 --workspace /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/experiments_outputs/2025_03_20_13_56_16 --st-neural-art default@../../application_code/object_detection/STM32N6/Model/user_neuralart.json --input-data-type uint8 --inputs-ch-position chlast
ST Edge AI Core v2.0.0-20049
PASS: 0%| | 0/82 [00:00<?, ?it/s]
PASS: 9%|▊ | 7/82 [00:00<00:04, 15.86it/s]
PASS: 11%|█ | 9/82 [00:00<00:05, 12.90it/s]
PASS: 13%|█▎ | 11/82 [00:00<00:05, 12.68it/s]
PASS: 17%|█▋ | 14/82 [00:01<00:04, 14.12it/s]
PASS: 26%|██▌ | 21/82 [00:01<00:02, 23.07it/s]
PASS: 29%|██▉ | 24/82 [00:01<00:02, 20.97it/s]
PASS: 33%|███▎ | 27/82 [00:01<00:02, 19.90it/s]
PASS: 37%|███▋ | 30/82 [00:01<00:02, 18.26it/s]
PASS: 39%|███▉ | 32/82 [00:01<00:02, 17.69it/s]
PASS: 41%|████▏ | 34/82 [00:01<00:02, 17.63it/s]
PASS: 44%|████▍ | 36/82 [00:02<00:02, 17.23it/s]
PASS: 46%|████▋ | 38/82 [00:02<00:02, 17.30it/s]
PASS: 49%|████▉ | 40/82 [00:02<00:02, 17.31it/s]
PASS: 52%|█████▏ | 43/82 [00:02<00:02, 19.02it/s]
PASS: 55%|█████▍ | 45/82 [00:02<00:02, 18.37it/s]
PASS: 60%|█████▉ | 49/82 [00:02<00:01, 21.31it/s]
PASS: 63%|██████▎ | 52/82 [00:02<00:01, 20.05it/s]
PASS: 67%|██████▋ | 55/82 [00:03<00:01, 17.26it/s]
PASS: 70%|██████▉ | 57/82 [00:03<00:01, 16.71it/s]
PASS: 72%|███████▏ | 59/82 [00:03<00:01, 16.15it/s]
PASS: 74%|███████▍ | 61/82 [00:03<00:01, 15.85it/s]
PASS: 77%|███████▋ | 63/82 [00:03<00:01, 14.18it/s]
PASS: 80%|████████ | 66/82 [00:03<00:00, 16.11it/s]
PASS: 84%|████████▍ | 69/82 [00:03<00:00, 17.32it/s]
PASS: 87%|████████▋ | 71/82 [00:04<00:00, 16.69it/s]
PASS: 89%|████████▉ | 73/82 [00:04<00:00, 16.22it/s]
>>>> EXECUTING NEURAL ART COMPILER
PASS: 89%|████████▉ | 73/82 [00:06<00:00, 16.22it/s]
/opt/ST/STEdgeAI/2.0/Utilities/linux/atonn -i "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/experiments_outputs/2025_03_20_13_56_16/ssd_mobilenet_v2_fpnlite_035_192_int8_OE_3_1_0.onnx" --json-quant-file "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/experiments_outputs/2025_03_20_13_56_16/ssd_mobilenet_v2_fpnlite_035_192_int8_OE_3_1_0_Q.json" -g "network.c" --load-mdesc "/opt/ST/STEdgeAI/2.0/Utilities/configs/stm32n6.mdesc" --load-mpool "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/Model/my_mpools/stm32n6-app2.mpool" --save-mpool-file "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/experiments_outputs/2025_03_20_13_56_16/neural_art__network/stm32n6-app2.mpool" --out-dir-prefix "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/experiments_outputs/2025_03_20_13_56_16/neural_art__network/" --all-buffers-info --no-hw-sw-parallelism --cache-maintenance --enable-virtual-mem-pools --native-float --optimization 3 --Os --Omax-ca-pipe 4 --Ocache-opt --enable-epoch-controller --output-info-file "c_info.json"
PASS: 89%|████████▉ | 73/82 [00:06<00:00, 16.22it/s]
Unable to execute the command "['/opt/ST/STEdgeAI/2.0/Utilities/linux/atonn', '-i', '/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/experiments_outputs/2025_03_20_13_56_16/ssd_mobilenet_v2_fpnlite_035_192_int8_OE_3_1_0.onnx', '--json-quant-file', '/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/experiments_outputs/2025_03_20_13_56_16/ssd_mobilenet_v2_fpnlite_035_192_int8_OE_3_1_0_Q.json', '-g', 'network.c', '--load-mdesc', '/opt/ST/STEdgeAI/2.0/Utilities/configs/stm32n6.mdesc', '--load-mpool', '/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/Model/my_mpools/stm32n6-app2.mpool', '--save-mpool-file', '/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/experiments_outputs/2025_03_20_13_56_16/neural_art__network/stm32n6-app2.mpool', '--out-dir-prefix', '/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/experiments_outputs/2025_03_20_13_56_16/neural_art__network/', '--all-buffers-info', '--no-hw-sw-parallelism', '--cache-maintenance', '--enable-virtual-mem-pools', '--native-float', '--optimization', '3', '--Os', '--Omax-ca-pipe', '4', '--Ocache-opt', '--enable-epoch-controller', '--output-info-file', 'c_info.json']"
[Errno 13] Permission denied: '/opt/ST/STEdgeAI/2.0/Utilities/linux/atonn'
PASS: 89%|████████▉ | 73/82 [00:06<00:00, 16.22it/s]
E103(CliRuntimeError): Error calling the Neural Art compiler - []
Error executing job with overrides: []
Traceback (most recent call last):
File "/home/anhem/miniconda3/envs/stm_32/lib/python3.10/site-packages/clearml/binding/hydra_bind.py", line 230, in _patched_task_function
return task_function(a_config, *a_args, **a_kwargs)
File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/stm32ai_main.py", line 228, in main
process_mode(cfg)
File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/stm32ai_main.py", line 102, in process_mode
deploy(cfg)
File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/../deployment/deploy.py", line 111, in deploy
stm32ai_deploy_stm32n6(target=board, stlink_serial_number=stlink_serial_number, stm32ai_version=stm32ai_version, c_project_path=c_project_path,
File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/../../common/deployment/common_deploy.py", line 515, in stm32ai_deploy_stm32n6
stmaic_local_call(session)
File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/../../common/deployment/common_deploy.py", line 489, in stmaic_local_call
stmaic.compile(session=session, options=opt, target=session._board_config)
File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/../../common/stm32ai_local/compile.py", line 216, in cmd_compile
raise Exception('Error during compilation')
Exception: Error during compilationWhat I need to do to fix it? Thank you
2025-03-20 1:30 AM
Hello @Anhem ,
If you install X Cube AI first, it will install the ST Edge AI Core (and the NPU if you install it also) here:
C:\Users\your_user\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\10.0.0\Utilities\windows\stedegeai.exe
If you use the standalone installer, I believe it install it in C:\ST\stedgeai\2.0.0\utilities\windows\stedgeai.exe
They are the same thing.
And because they are the same thing, if you install X Cube AI after installing the standalone, it will not install it again but use the second path I wrote.
I do think that the standalone installer doesn't look out for another version installed on your PC. It will install it no matter what, but I did not test it out.
Have a good day,
Julian
2025-03-20 2:57 AM
Hi @Julian E.
@Julian E. wrote:Hello @Anhem ,
If you install X Cube AI first, it will install the ST Edge AI Core (and the NPU if you install it also) here:
C:\Users\your_user\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\10.0.0\Utilities\windows\stedegeai.exe
If you use the standalone installer, I believe it install it in C:\ST\stedgeai\2.0.0\utilities\windows\stedgeai.exe
They are the same thing.
And because they are the same thing, if you install X Cube AI after installing the standalone, it will not install it again but use the second path I wrote.
I do think that the standalone installer doesn't look out for another version installed on your PC. It will install it no matter what, but I did not test it out.
Have a good day,
Julian
That is cleared for me.
Could you give advice for the above error when I tried deploying tflite model on the board?
2025-03-20 3:02 AM
Hello @Anhem ,
Can you send me your user_config.yaml please.
Concerning the graphic card, did you get an error ? the code should use a GPU if it finds one, but should still works even if you don't have one.
In terms of steps while setting up everything, can you confirm that you:
Julian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.