2020-09-11 7:19 AM
Hi,
We are working to an ANN development on TensorFlow, this ANN works on computer and not on MCU.
During implementation throught CubeMX, an estimation of RAM and Flash permit to select an appropriate MCU.
My question is, ANN implementation is only available if we use internal RAM and Flash or we can run ANN on external RAM ?
BR,
Solved! Go to Solution.
2020-09-11 7:39 AM
On the network view you have an additional popup window (with the button) where you can ask to use external memories.
On STM32 known boards, if there is external memory, it will automatically insert the BSP code to use that memory in the generated code.
If you use external memory you can ignore the message that the amount of RAM / Flash required is bigger than the one availbale
When using external memory, the weights are located in external memory and a network_data.bin file is generated so you can flash it on the external memory
The same applies for external RAM, you can put the activation buffer in external RAM
Regards
Daniel
2020-09-11 7:39 AM
On the network view you have an additional popup window (with the button) where you can ask to use external memories.
On STM32 known boards, if there is external memory, it will automatically insert the BSP code to use that memory in the generated code.
If you use external memory you can ignore the message that the amount of RAM / Flash required is bigger than the one availbale
When using external memory, the weights are located in external memory and a network_data.bin file is generated so you can flash it on the external memory
The same applies for external RAM, you can put the activation buffer in external RAM
Regards
Daniel
2020-09-16 1:02 AM
Hi,
Thank you for this precision,
Regards,
Benjamin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.