2020-09-13 11:26 AM
I confronted an error "TOOL ERROR: (1, 4, 12, 10) is not a permutation for (2, 0, 1)"
It seems there's some issues with handling the model structure. But I can't figure it out.
The model perfectly works on python and the structure is not so different from models which had been successfully imported to the my board (NUCLEO-L452RE)
The tool version is X-CUBE-AI 5.1.2 and I'm using the STM32CubeMX GUI.
The model has the structure shown below (checked by model.summary())
_________________________________________________________________
Layer (type) Output Shape Param #
=================================================================
input_8 (InputLayer) [(None, 36, 100, 1)] 0
_________________________________________________________________
conv2d_16 (Conv2D) (None, 36, 100, 5) 130
_________________________________________________________________
average_pooling2d_5 (Average (None, 9, 25, 5) 0
_________________________________________________________________
re_lu_14 (ReLU) (None, 9, 25, 5) 0
_________________________________________________________________
conv2d_17 (Conv2D) (None, 9, 25, 10) 1260
_________________________________________________________________
max_pooling2d_9 (MaxPooling2 (None, 4, 12, 10) 0
_________________________________________________________________
re_lu_15 (ReLU) (None, 4, 12, 10) 0
_________________________________________________________________
flatten_1 (Flatten) (None, 480) 0
_________________________________________________________________
dense_5 (Dense) (None, 6) 2886
_________________________________________________________________
softmax_1 (Softmax) (None, 6) 0
=================================================================
Total params: 4,276
Trainable params: 4,276
Non-trainable params: 0
_________________________________________________________________
The structure shown below is successfully anaylized.
------------------------------------------------------------------------------------------------------------------------
id layer (type) output shape param # connected to macc rom
------------------------------------------------------------------------------------------------------------------------
0 input_2 (Input) (16, 100, 1)
conv2d_0 (Conv2D) (16, 100, 5) 130 input_2 208,005 520
------------------------------------------------------------------------------------------------------------------------
1 pool_1 (Pool) (4, 25, 5) conv2d_0
nl_1 (Nonlinearity) (4, 25, 5) pool_1 500
------------------------------------------------------------------------------------------------------------------------
2 conv2d_2 (Conv2D) (4, 25, 10) 1,260 nl_1 125,970 5,040
------------------------------------------------------------------------------------------------------------------------
3 pool_3 (Pool) (2, 12, 10) conv2d_2
nl_3 (Nonlinearity) (2, 12, 10) pool_3 240
------------------------------------------------------------------------------------------------------------------------
4 conv2d_4 (Conv2D) (2, 12, 6) 546 nl_3 13,110 2,184
------------------------------------------------------------------------------------------------------------------------
5 pool_5 (Pool) (1, 1, 6) conv2d_4
------------------------------------------------------------------------------------------------------------------------
6 nl_6 (Nonlinearity) (1, 1, 6) pool_5 90
------------------------------------------------------------------------------------------------------------------------
Solved! Go to Solution.
2020-09-14 11:56 PM
Hello HKim,
I suppose that you use a tflite model which has been converted from a Keras model in a TFensorFlow 2.2 or later environment. If you confirm, this issue is in a change of the behavior of TFLiteConverter (vs TF 1.15 or 2.0) which managed differently the conversion of the dense layer (including the flatten operator). Now a reshape tflite operator is systematically introduced. Unfortunately, in X-CUBE-AI 5.1.2, this change has not be fully fixed and with a 3-dim input shape, this error can appear. This issue is now fixed and will be delivery in the X-CUBE-AI 5.2.0 release.
Do you confirm my analysis about the usage of the TFLite model? If not, is it possible to have more details about the imported model, environment used to generate the model: Keras?, TFlite? Is it possible to share the model file imported in X-CUBE-AI?
br,
Jean-Michel
2020-09-14 11:56 PM
Hello HKim,
I suppose that you use a tflite model which has been converted from a Keras model in a TFensorFlow 2.2 or later environment. If you confirm, this issue is in a change of the behavior of TFLiteConverter (vs TF 1.15 or 2.0) which managed differently the conversion of the dense layer (including the flatten operator). Now a reshape tflite operator is systematically introduced. Unfortunately, in X-CUBE-AI 5.1.2, this change has not be fully fixed and with a 3-dim input shape, this error can appear. This issue is now fixed and will be delivery in the X-CUBE-AI 5.2.0 release.
Do you confirm my analysis about the usage of the TFLite model? If not, is it possible to have more details about the imported model, environment used to generate the model: Keras?, TFlite? Is it possible to share the model file imported in X-CUBE-AI?
br,
Jean-Michel
2020-10-11 8:47 AM
Hello Mr. Jean-Michel
Thanks for your detailed explanation.
As you mentioned, my model was tflite model converted from Keras model using TFLiteConverter. But I'm not sure the issue had come from TFLiteConverter API. Anyway, I just checked this issue didn't appear in X-CUBE-AI version 5.2.0.
Best regards,
HKim.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.