2026-02-17 8:25 AM - edited 2026-02-18 12:18 AM
Hello,
I am experimenting with X-Cube-AI (v10.2.0) in STM32CubeMX(v6.16.1). I noted that the version of the ST Edge AI Core in this case is v2.2.0. Moreover, this makes that the Embedded Interface is the legacy one, instead of the the newest ST-AI. I wonder if there are plans to update X-Cube-AI so it uses the latest version of ST Edge AI (v3.0.0), and uses the latest the ST-AI interface.
Thanks.
Solved! Go to Solution.
2026-02-19 6:22 AM
See this post, X-Cube-AI was replaced by STM32Cube AI Studio yesterday.
2026-02-19 6:22 AM
See this post, X-Cube-AI was replaced by STM32Cube AI Studio yesterday.
2026-02-19 7:04 AM - edited 2026-02-19 7:04 AM
Hi,
Exactly, X Cube AI is no longer updated. It was replaced by STM32CubeAI studio, a desktop app.
You can use the ST Edge AI Core version 2.2 and later with it.
Make sure to update all the required dependencies.
Have a good day,
Julian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.