2025-04-10 7:44 AM - edited 2025-04-15 9:33 AM
Hi everyone,
I'm trying to run inference with a TFLite model on a Nucleo-N657X0-Q board.
The issue I'm facing is that the network returns a constant output for constant inputs - but the value of this constant changes each time I restart the application. When the input varies, the output also varies, but the values returned are not consistent with those obtained during the validation process.
The model was quantized using a post-training quantization approach.
I'm using AXISRAM4 and AXISRAM5, which have been correctly initialized and enabled in the main.c.
I attach the .ioc file, the app_x-cube-ai.c file and the quantized tflite model for reference.
Thanks in advance for any suggestions!
Solved! Go to Solution.
2025-04-14 8:15 AM
Hello Lisa,
Thanks for your feedback.
For the external flash, maybe you can take a look at examples provided with the Neural-Art component.
In order to easily read the external flash, you need to "memory-map" it, the easiest way for development boards being to make use of the BSP functions like BSP_XSPI_NOR_Init...
Take a look at project examples on how to memory-map external memories !
Storing weights in flash should make your life easier and should fix the issues you had above with unstable outputs (because of unstable weights :) ).
2025-04-15 1:46 AM - edited 2025-04-15 8:10 AM
2025-04-28 2:27 AM - edited 2025-05-05 3:50 AM
Hi,
I am having a similar problem, I am trying to save the weights of my AI model in the external Flash. I do not know if what I have done so far is correct but I am able to build the project. The problem is that the FSBL and AppN projects run successfully but when I run or debug the AppNS project, where the AI related code is located, I get debugger connection errors and it seems like the debugger never gets connected to the board.
So my question is, how did you save the weights to the external flash @LisaB ? Is it possible for you to help me?
Thanks!
2025-05-05 12:19 AM
Hello @fa31,
Sorry for the late reply.
The suggestion I received from ST was to work only in the FSBL for simplicity, if possible.
2025-05-05 3:49 AM
Hi @LisaB ,
Thank you for the reply!
But even though you had everything in the FSBL project, did you use the external flash to save the AI-model?
2025-05-05 4:50 AM
Hello @fa31,
Yes, I used the external flash.
Once you validate your model on the target, a .hex file is generated in the folder:
C:\Users\Name\.stm32cubemx\network_output.
The network weights are correctly flashed into memory once you perform the Validation on target or by using the .hex file with CubeProgrammer.
Hope this helps!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.