2022-03-15 7:00 AM
/* USER CODE BEGIN PV */
static ai_buffer *ai_input;
static ai_buffer *ai_output;
/* USER CODE END PV */
int main(void){
...
// Chunk of memory used to hold the intermediate values for neural network
AI_ALIGNED(32) ai_u32 activations[AI_NETWORK_DATA_ACTIVATIONS_SIZE];
// Buffers used to store input and output tensors
AI_ALIGNED(32) ai_i32 in_data[AI_NETWORK_IN_1_SIZE_BYTES];
AI_ALIGNED(32) ai_i32 out_data[AI_NETWORK_OUT_1_SIZE_BYTES];
// Pointer to our model
ai_handle my_model = AI_HANDLE_NULL;
// structs that point to our input and output data and some meta data
ai_input = ai_network_inputs_get(my_model , NULL);
ai_output = ai_network_outputs_get(my_model , NULL);
....
}As seen the function ai_network_inputs_get(ai_handle network, ai_u16 *n_buffer) resides in the network.c file and it makes a call to the ai_platform_inputs_get(network, n_buffer); in file ai_platform_interface.h
It doesnt give me any errors while running but the code breaks while getting the ai_buffer to the input of the model
I dont know what possibly can go wrong. Should I explicitally implement these functions in main() ? There exists some literature and videos on web but they are old.
Is there anyone who has faced similar problems or knows solutioon to this?
Thanks in advance
2022-03-16 3:39 AM
Alright, I think I found the solution to the problem.
The problem is before calling the ai_network_inputs_get function the ai model has to be created.
So the solution looks like this
/* USER CODE BEGIN PV */
static ai_buffer *ai_input;
static ai_buffer *ai_output;
/* USER CODE END PV */
int main(void){
...
// Chunk of memory used to hold the intermediate values for neural network
AI_ALIGNED(32) ai_u32 activations[AI_NETWORK_DATA_ACTIVATIONS_SIZE];
// Buffers used to store input and output tensors
AI_ALIGNED(32) ai_i32 in_data[AI_NETWORK_IN_1_SIZE_BYTES];
AI_ALIGNED(32) ai_i32 out_data[AI_NETWORK_OUT_1_SIZE_BYTES];
// Pointer to our model
ai_handle my_model = AI_HANDLE_NULL;
..........
/* USER CODE BEGIN 2 */
..........
ai_network_params ai_params =
{
{
AI_NETWORK_DATA_WEIGHTS(ai_network_data_weights_get()),
AI_NETWORK_DATA_ACTIVATIONS(activations)
}
};
// Create instance of the neural network
ai_err = ai_network_create(&my_model, AI_NETWORK_DATA_CONFIG);
if (ai_err.type != AI_ERROR_NONE)
{
buf_len = sprintf(buf, "Error: Could not create NN instance\r\n");
HAL_UART_Transmit(&huart3, (uint8_t *)buf, buf_len, 100);
while(1);
}
// Initialize neural network. At this point we are ready to make inferences
if (!ai_network_init(my_model, &ai_params))
{
buf_len = sprintf(buf, "Error: could not initialize NN\r\n");
HAL_UART_Transmit(&huart3, (uint8_t *)buf, buf_len, 100);
while(1);
}
// structs that point to our input and output data and some meta data
ai_input = ai_network_inputs_get(my_model, NULL);
ai_output = ai_network_outputs_get(my_model, NULL);
....
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.