2025-03-15 2:25 AM
Good day,
preparing to an online workshop I am trying to install prerequisites. However the component en.stedgeai-stneuralart-10.0.0.zip does not install, STM32CibeIDE says: "This file is either corrupted or not a recognized package.".
Regards,
Dmitry
2025-03-17 1:04 AM
Hello @DmitryR ,
You are installing X Cube AI (and npu) with the integrated CubeMX in CubeIDE?
Make sure to use STM32CubeIDE v1.17.0 minimum.
Then you can try to eitheir uninstall X Cube AI v10.0.0 and then install it again in STM32CubeMX
Or uninstall X Cube AI v10, install the st edge ai core as standalone (where you downloaded the stneuralart) and install X Cube AI after that, as he will use the standalone st edge ai core.
Have a good day,
Julian
2025-03-26 12:30 AM
Hi @Julian E. ,
do you mean that the X-Cube-AI v. 10.0.0 is the same as en.stedgeai-stneuralart-10.0.0.zip download?
Regards,
Dmitry
2025-03-26 12:54 AM
Hello,
The zip file en.stedgeai-stneuralart-10.0.0.zip is a component that you will need to install directly from X-CUBE-AI. You need first to install X-CUBE-AI 10.0.0, and once you open a board with ST Neural-ART Accelerator (such as STM32N6570-DK) you will be asked to install ST Neural-ART package if not available. You will enter your zip when asked.
How to install X-CUBE-AI:
AI:How to install X-CUBE-AI through STM32CubeMX - stm32mcu
If you select STM32N6570-DK instead of NUCLEO like the documentation, you will have a pop-up asking for en.stedgeai-stneuralart-10.0.0.zip
Hope its clearer
Best regards,
Yanis
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.