2021-11-22 7:10 AM
Hello,
I'm having some problems using Unico-GUI to configure the MLC of an LSM6DSOX. I'm trying to develop an application using four filters (actually, the same filter applied on the XYZ and V signals of the Accelerometer and Gyroscope), but the Unico software doesn't allow me to select more than 31 features.
I'm using Unico-GUI (STSW-MKI109M) on a Macintosh machine with macOS Monterey Version 12.0.1. I have tried both versions of Unico-GUI (9.11.0 and 9.10.0), and I have always gotten the same problem.
How can I configure the software to select a higher number of features?
Thanks for your help!
Solved! Go to Solution.
2021-11-23 5:04 AM
Hi @henryjhoán Areiza Laverde ,
please consider that the statement in the AN5259 application note, p.9.
Note: The maximum number of features which can be configured in the MLC is 31.
This means that on ST devices the MLC limitations in terms of features are:
This limitation is both for Unico and for the script running behind it.
There might in any case be some possible workarounds that might fit your case:
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-11-23 5:04 AM
Hi @henryjhoán Areiza Laverde ,
please consider that the statement in the AN5259 application note, p.9.
Note: The maximum number of features which can be configured in the MLC is 31.
This means that on ST devices the MLC limitations in terms of features are:
This limitation is both for Unico and for the script running behind it.
There might in any case be some possible workarounds that might fit your case:
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.