cancel
Showing results for 
Search instead for 
Did you mean: 

Interaction between accelerometer and pretrained NN in STM32F7

HKili.16
Associate

Hello,

 

https://www.youtube.com/watch?v=grgNXdkmzzQ in this video, your collegue describes how to implement a keras model into the STM32Cube A.I and a STM32F7. My further step:

 

assuming i measure further values with the same accelerometer with the pretrained NN programmed STM32F7 via I2C. Now this model is trained via Keras for different classes (sitting, jogging, running, walking etc.) . When i measure values via I2C through the pretrained Microcontroller through the model, how can i distinguish between these different classes within the microcontroller?. Because i think this pretrained NN which is into the microcontroller should recognize these classes, isnt it?.

For example i would express through a Uart-port these classes to a terminal. How should that work?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
fauvarque.daniel
ST Employee

The function pack "STM32Cube function pack for ultra-low power IoT node with artificial intelligence (AI) application based on audio and motion sensing" available here gives you an example of a real application using external sensors and X-Cube-AI.

Regards

Daniel


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.