2025-02-28 1:35 AM
Hi everyone,
I am trying to deploy a pose detection model on stm32n6570-dk board but I am getting the following error.
(st_zoo) kartikkhandewal@ATL-HPZG14-99:~/stm32packages/stm32ai-modelzoo-services/pose_estimation/src$ python3 stm32ai_main.py --config-path ./config_file_examples --config-name deployment_n6_yolo_mpe_config.yaml
WARNING: All log messages before absl::InitializeLog() is called are written to STDERR
E0000 00:00:1740729082.336274 136562 cuda_dnn.cc:8310] Unable to register cuDNN factory: Attempting to register factory for plugin cuDNN when one has already been registered
E0000 00:00:1740729082.339482 136562 cuda_blas.cc:1418] Unable to register cuBLAS factory: Attempting to register factory for plugin cuBLAS when one has already been registered
[WARNING] The usable GPU memory is unlimited.
Please consider setting the 'gpu_memory_limit' attribute in the 'general' section of your configuration file.
[INFO] : Running `deployment` operation mode
[INFO] : The random seed for this simulation is 123
INFO: Created TensorFlow Lite XNNPACK delegate for CPU.
[INFO] : Generating C header file for Getting Started...
loading model.. model_path="yolov8n_256_quant_pc_uf_pose_pallet.tflite"
loading conf file.. "../../application_code/pose_estimation/STM32N6/stmaic_STM32N6570-DK.conf" config="None"
"n6 release" configuration is used
[INFO] : Selected board : "STM32N6570-DK Getting Started Pose Estimation (STM32CubeIDE)" (stm32_cube_ide/n6 release/stm32n6)
[INFO] : Compiling the model and generating optimized C code + Lib/Inc files: yolov8n_256_quant_pc_uf_pose_pallet.tflite
setting STM.AI tools.. root_dir="", req_version=""
Cube AI Path: "/home/kartikkhandewal/STEdgeAI/2.0/Utilities/linux/stedgeai".
[INFO] : Offline CubeAI used; Selected tools: 10.0.0 (x-cube-ai pack)
loading conf file.. "../../application_code/pose_estimation/STM32N6/stmaic_STM32N6570-DK.conf" config="None"
"n6 release" configuration is used
compiling... "yolov8n_256_quant_pc_uf_pose_pallet_tflite" session
model_path : ['yolov8n_256_quant_pc_uf_pose_pallet.tflite']
tools : 10.0.0 (x-cube-ai pack)
target : "STM32N6570-DK Getting Started Pose Estimation (STM32CubeIDE)" (stm32_cube_ide/n6 release/stm32n6)
options : --st-neural-art default@../../application_code/pose_estimation/STM32N6/Model/user_neuralart.json --input-data-type uint8 --inputs-ch-position chlast
"series" value is not coherent.. stm32n6 != stm32n6npu
results -> RAM=1,675,264 IO=196,608:220,416 WEIGHTS=3,243,377 MACC=0 RT_RAM=1,893 RT_FLASH=504,138 LATENCY=0.000
[INFO] : Optimized C code + Lib/Inc files generation done.
[INFO] : Building the STM32 c-project..
deploying the c-project.. "STM32N6570-DK Getting Started Pose Estimation (STM32CubeIDE)" (stm32_cube_ide/n6 release/stm32n6)
updating.. n6 release
-> s:copying file.. "network.c" to ../../application_code/pose_estimation/STM32N6/Model/network.c
-> s:copying file.. "network_ecblobs.h" to ../../application_code/pose_estimation/STM32N6/Model/network_ecblobs.h
-> s:copying file.. "network_atonbuf.xSPI2.raw" to ../../application_code/pose_estimation/STM32N6/Model/network_atonbuf.xSPI2.raw
-> s:removing dir.. ../../application_code/pose_estimation/STM32N6/Middlewares/AI_Runtime/Lib/GCC/ARMCortexM55
-> s:copying dir.. "ARMCortexM55" to ../../application_code/pose_estimation/STM32N6/Middlewares/AI_Runtime/Lib/GCC/ARMCortexM55
-> s:removing dir.. ../../application_code/pose_estimation/STM32N6/Middlewares/AI_Runtime/Inc
-> s:copying dir.. "Inc" to ../../application_code/pose_estimation/STM32N6/Middlewares/AI_Runtime/Inc
-> s:removing dir.. ../../application_code/pose_estimation/STM32N6/Middlewares/AI_Runtime/Npu/ll_aton
-> s:copying dir.. "ll_aton" to ../../application_code/pose_estimation/STM32N6/Middlewares/AI_Runtime/Npu/ll_aton
-> u:copying file.. "app_config.h" to ../../application_code/pose_estimation/STM32N6/Inc/app_config.h
-> updating cproject file "/home/kartikkhandewal/stm32packages/stm32ai-modelzoo-services/application_code/pose_estimation/STM32N6/STM32CubeIDE" with "NetworkRuntime1000_CM55_GCC.a"
building.. n6 release
[returned code = 1 - FAILED]
flashing.. n6 release STM32N6570-DK
[returned code = 1 - FAILED]
Board programming failed: " Error: binary file does not exist: Debug/STM32N6_GettingStarted_PoseEstimation.bin"
[returned code = 1 - FAILED]
Board programming failed: "Error: File does not exist: STM32N6_GettingStarted_PoseEstimation_signed.bin"
Board programming failed: "Error: File does not exist: STM32N6_GettingStarted_PoseEstimation_signed.bin"
Board programming failed: "Error: File does not exist: STM32N6_GettingStarted_PoseEstimation_signed.bin"
[INFO] : Deployment complete.
[INFO] : Please on STM32N6570-DK toggle the boot switches to the left and power cycle the board.
I have deployed object detection models on board and they have worked fine but I am not able to deploy this.
Steps I followed-
best.pt ----> my original pose detection model (12 keypoints to detect)
converted it to tflite which gave me saved_model using
from ultralytics import YOLO
model_path = 'best.pt'
model = YOLO(model_path)
results = model.export(format='tflite', int8=True, imgsz=[256, 256])
Quantized model following this tutorial .
Deployed it using this tutorial
Kindly help.
Solved! Go to Solution.
2025-07-14 10:37 PM
Solved
The current model-zoo scripts only support YOLOv8n-pose models with 17 keypoints by default. If you are using any other keypoint model (with a different number of keypoints), you will need to modify the code manually.
Specifically, you must create a new header file named display_keypoint_<number_of_points>.h corresponding to your model’s keypoint count, and include it in the codebase accordingly. See display_keypoint_17.h on how to do it in code.
Mode-zoo version - v3.0.0
2025-03-04 2:40 AM
Hello @athern27 ,
The issue may come from the 12 keypoints to detect. It seems that we only support 13 and 17.
Can you try to use a model with 13 or 17 keypoints?
You can find ultralytics yolos model examples here:
ultralytics/examples/YOLOv8-STEdgeAI at main · stm32-hotspot/ultralytics
If it doesn't help, it may be an issue in the deployment scripts, so do not hesitate to come back to me if you still have an issue.
Have a good day,
Julian
2025-03-04 10:10 PM
Hi @Julian E. ,
I tried running the yolov8n-pose.pt model, which is designed to detect 17 body keypoints. After quantizing it, I was able to run it successfully with good accuracy.
Is there no way to deploy a 12-keypoint model on the board?
Kindly help.
2025-03-06 5:40 AM
Hello @athern27,
I am not exactly sure about the procedure, could you please try to adapt the postprocess_conf.h with
And look at the need app.c and see if you see something related to that.
I've got the information that it is not a big deal to change the getting started but I don't have clear guideline.
If you can generate a model with 17 and 13 keypoints and compare what is different, you may be able to understand the part related to the keypoints.
Have a good day,
Julian
2025-07-14 10:37 PM
Solved
The current model-zoo scripts only support YOLOv8n-pose models with 17 keypoints by default. If you are using any other keypoint model (with a different number of keypoints), you will need to modify the code manually.
Specifically, you must create a new header file named display_keypoint_<number_of_points>.h corresponding to your model’s keypoint count, and include it in the codebase accordingly. See display_keypoint_17.h on how to do it in code.
Mode-zoo version - v3.0.0
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.