2024-03-21 4:03 AM
Hi all,
I'm trying add FPU exception to my project and I'm bit confused because two sources points two different interrupt vectors for this. Book E says, FPU exception is under IVOR33 but SPC58xH manual points IVOR10. And SPC5Studio libraries have "decrementer support" under IVOR10. I suspect SPC58xH is right for me but I want to be sure.
regards
Michal
Solved! Go to Solution.
2024-04-13 5:51 AM
Hello,
SPC58xH Reference Manual is right.
SPC58xH implements two FPU exceptions:
Each entry in the exception table is 16 bytes.
Considering the exception table as an array with 16 bytes for each entry:
In SPC5Studio, exception table implementation uses align 4 directive to have 16 bytes displacement.
SPC5Studio implements the exception table up to entry 15 (IVOR15)
IVOR10 implementation, in SPC5Studio, refers to the decrementer as defined on Book-E but the code is commented, just a matter of porting the exception handlers form a previous device (which implements the decrementer at IVOR10).
Best Regards.
2024-03-22 10:01 AM
Hello ,
i am checking the mismatch between booke and SPC58Hx Ref Manual
by default , take Chorus_10M Reference Manual ;)
Best regards
Erwan
2024-03-29 8:33 AM
Hi Erwan,
I've found bug in application note AN5549 where figures 6 and 10 should be swapped.
Hardware vector mode require vector table at offset 0x1000 so fig. 10 is incorrect.
regards
Michal
2024-04-13 5:51 AM
Hello,
SPC58xH Reference Manual is right.
SPC58xH implements two FPU exceptions:
Each entry in the exception table is 16 bytes.
Considering the exception table as an array with 16 bytes for each entry:
In SPC5Studio, exception table implementation uses align 4 directive to have 16 bytes displacement.
SPC5Studio implements the exception table up to entry 15 (IVOR15)
IVOR10 implementation, in SPC5Studio, refers to the decrementer as defined on Book-E but the code is commented, just a matter of porting the exception handlers form a previous device (which implements the decrementer at IVOR10).
Best Regards.
2024-04-16 4:53 AM
Is it necessary switch to hardware vector mode to support FPU exception in IVOR10?
regards
Michal
2024-04-16 5:20 AM
Hello Michal,
there is no need to switch to hardware mode interrupt to handle IVOR10 exception.
Please have a look at SPC58NH Reference Manual rev4, at page 450.
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.