2021-01-23 1:00 AM
Hi guys,
i have the following problem.
I configure the interrupts as follow.
INTC.BCR.R = 0;
INTC.IACKR[0].R = (uint32_t)&VectorTable[0];
INTC.CPR[0].B.PRI = 0;
// enable interrupts
__asm__ volatile ("wrteei 1" : : : "memory");After that, i configure one Etimer Channel with timer compare interrupt. The interrupt flag will set in etimer module, but the ISR will never be called.
If i change my configuration to the following, the interrupts will come:
INTC.BCR.R = 0;
INTC.IACKR[0].R = (uint32_t)&VectorTable[0];
(void)INTC.IACKR[0].R; // read back
INTC.CPR[0].B.PRI = 0;
// enable interrupts
__asm__ volatile ("wrteei 1" : : : "memory");I would be happy if someone could explain what I'm doing wrong, because I can't find anything about it in the reference manual.
best regards
david
Solved! Go to Solution.
2021-02-02 8:43 AM
Dear All ,
Sorry, difficult for me to support Hightec IDE on irq handler .
Could you give me the HW used ?
could you check in SPC5Studio 6.0 (spc574kxx_irq_component_rla) (cf below)?
there is a nice irq handler.
/**
* @brief IRQ module initialization.
*
* @api
*/
void irqInit(void) {
irq_cfg_init();
/* Method of accessing memory-mapped registers at fixed addresses does not
comply with MISRA C because it involves converting an integer to a
pointer. */
/*lint -e9033 */
/* INTC initialization, software vector mode, 4 bytes vectors, starting
at priority 0.*/
INTC_BCR = 0;
/* Configure IRQ for main core.*/
INTC_CPR(MAIN_CORE) = 0;
INTC_IACKR(MAIN_CORE) = (uint32_t)_vectors;
#if defined(BOOT_CORE0) && (BOOT_CORE0 == 1)
/* Configure IRQ for secondary core 0.*/
INTC_CPR(0) = 0;
INTC_IACKR(0) = (uint32_t)_vectors;
#endif /* BOOT_CORE0 */
#if defined(BOOT_CORE1) && (BOOT_CORE1 == 1)
/* Configure IRQ for secondary core 1.*/
INTC_CPR(1) = 0;
INTC_IACKR(1) = (uint32_t)_vectors;
#endif /* BOOT_CORE1 */
#if defined(BOOT_CORE2) && (BOOT_CORE2 == 1)
/* Configure IRQ for secondary core 2.*/
INTC_CPR(2) = 0;
INTC_IACKR(2) = (uint32_t)_vectors;
#endif /* BOOT_CORE2 */
/*lint +e9033 */
}Best regards
Erwan
2021-02-02 8:43 AM
Dear All ,
Sorry, difficult for me to support Hightec IDE on irq handler .
Could you give me the HW used ?
could you check in SPC5Studio 6.0 (spc574kxx_irq_component_rla) (cf below)?
there is a nice irq handler.
/**
* @brief IRQ module initialization.
*
* @api
*/
void irqInit(void) {
irq_cfg_init();
/* Method of accessing memory-mapped registers at fixed addresses does not
comply with MISRA C because it involves converting an integer to a
pointer. */
/*lint -e9033 */
/* INTC initialization, software vector mode, 4 bytes vectors, starting
at priority 0.*/
INTC_BCR = 0;
/* Configure IRQ for main core.*/
INTC_CPR(MAIN_CORE) = 0;
INTC_IACKR(MAIN_CORE) = (uint32_t)_vectors;
#if defined(BOOT_CORE0) && (BOOT_CORE0 == 1)
/* Configure IRQ for secondary core 0.*/
INTC_CPR(0) = 0;
INTC_IACKR(0) = (uint32_t)_vectors;
#endif /* BOOT_CORE0 */
#if defined(BOOT_CORE1) && (BOOT_CORE1 == 1)
/* Configure IRQ for secondary core 1.*/
INTC_CPR(1) = 0;
INTC_IACKR(1) = (uint32_t)_vectors;
#endif /* BOOT_CORE1 */
#if defined(BOOT_CORE2) && (BOOT_CORE2 == 1)
/* Configure IRQ for secondary core 2.*/
INTC_CPR(2) = 0;
INTC_IACKR(2) = (uint32_t)_vectors;
#endif /* BOOT_CORE2 */
/*lint +e9033 */
}Best regards
Erwan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.