2023-07-26 11:55 PM
I'd like to enquire on one of the application notes for EV pyro fuse. Can it be made standalone/self-triggered?
Here is the application note;
shubhash
2023-08-28 8:33 AM
Hello ,
According the the AN
This device is family compatible with the L9678,
L9680 and L9679P devices: it has been designed as extension chip of the others, but if configured in the right
way it can be used standalone.
what do you mean about Self-Triggered ?
Best regards
Erwan
2023-09-11 2:34 PM - edited 2023-09-11 2:36 PM
I have a similar if not the same question. I have been tasked with doing a design in a few weeks that needs to fire Pyro Fuses when current sensors assert their overcurrent fault flag. I've been told that this needs to be on the order of 50uS so a SPI message would be too slow. From what I can tell the L9679P and L9679e can be told through SPI to deploy and will wait for during the timeout period for a trigger signal.
It looks to me that this could be done using the FENL pin. Could the DCSx pins also cause the L9679P to trigger once a deploy command is sent?
Is there a better way to get this quick of trigger on an overcurrent?
Rob
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.