2016-02-17 2:46 AM
This time it's going to be really tough, so every suggestion is well appreciated.
I'm using SPC5 studio and I'd need to run some code just on a single core to avoid any kind of lockstep intervention. So, I need to configure the device in DPM. Flashing the device with a modified pattern in the shadow memory lets me connect it with JTAG in DPM with no problem.Then, starting from a LSM project, in the linker file i put 96 kB instead of 192 kB to handle with the DPM configuration. Now I'll need to add a different MMU initialization , as stated in http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00168395.pdf , but I don't know where. As it is, the MCU hangs at startup and the main is never entered.The main question is : is it feasibile, starting from a wizard project, of SPC5 studio for LSM to create a DPM working project?2016-02-24 2:21 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.