2016-04-27 1:19 AM
I try to use SPC56EL70L5-DISP(master) to communicate another board(slave) through SPI.
CRC-8 , polynomial, C(x) = x8 + x2 + x1 + 1 , is needed for the SPI last byte. I attempt to use the SPC56EL70L3 build-in CRC function to check/generate CRC byte. However the datasheet mentions it supports x8 + x4 + x3 + x2 + 1. Is it possible for me to use the built-in CRC function? And how do I configure the CRC reg(CRC_CFG, CRC_INP, CRC_CSTAT) Thanks for help #crc2016-04-27 1:53 AM
2016-04-27 8:31 PM
2016-04-28 12:29 AM
Hello Tony ,
you have to play with some filters to find the test application (cf screenshot) Best regards Erwan ________________ Attachments : 2016-04-28_092854.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0YA&d=%2Fa%2F0X0000000baF%2F06n9IAS73zgzOC6NW7B0Fl6S0D38rA3KB1oR5L7RaDE&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.